Part Number: SN74LVC32A
Dear TI Team,
We are using the SN74LVC32APWR quad OR gate in our design to combine two separate MCU output signals. The OR-gate output is used as the control signal for a transistor input.
Circuit description:
…
Part Number: SN74LVC32A I have a question regarding the input voltage of the SN74LVC series ICs. The datasheet specifies an absolute rating of -0.5 to +6.5V, but is there any tolerance for overshoot, where the voltage may drop below -0.5V for about 1…
Part Number: SN74LVC32A-Q1 Other Parts Discussed in Thread: SN74LVC32A Dear Sirs
I am looking for the IBIS Model of the SN74LVC32A-Q1. Is it avaliable?
Thanks a lot and regards
Salvatore
Part Number: SN74LVC32A Hi, is there a junction to board and/or junction to case thermal resistance value available for this part? The full P/N is
SN74LVC32ARGYR
Hi Thomas,
I split this thread since it's on a new device even though the topic is similar to Takahashi-san's post.
The absolute maximum ratings table for SN74LVC32A indicates that the supply can work up to 6.5V, so 5V would not be a problem.
…
Part Number: SN74LVC32A Other Parts Discussed in Thread: SN74LVC1G3157 , Hello Team,
Can you provide the Tjmax of our SN74LVC32A and SN74LVC1G3157 for long time work spec to me, there is no this spec in our datasheets? thanks.
Regards,
Nanfan…
Part Number: SN74LVC32A Hello team,
My customer use our SN74LVC32A, now they test the input signal and the Input transition rise and fall rate is 10ns/V, which is higher than 7ns/V(our spec), it is OK, any risk? thanks
Regards,
Nanfang
Part Number: SN74AVC2T244 Other Parts Discussed in Thread: SN74AVCH1T45 , , SN74LVC32A , SN74HCS32 , SN74LVC7032A Can I connect the outputs of several translators as an external "OR" gate using 1kOhm resistors?
How much current can the outputs sink…