Part Number: SN74LVC32A Hi, is there a junction to board and/or junction to case thermal resistance value available for this part? The full P/N is
SN74LVC32ARGYR
Part Number: SN74LVC32A-Q1 Other Parts Discussed in Thread: SN74LVC32A Dear Sirs
I am looking for the IBIS Model of the SN74LVC32A-Q1. Is it avaliable?
Thanks a lot and regards
Salvatore
Part Number: SN74LVC7032A Other Parts Discussed in Thread: SN74LVC32A Hi experts
We notice that we have a new series logic parts like SN74LVC7032A, what's the meaning of 70? What's the main difference between SN74LVC7032A and SN74LVC32A?
Other Parts Discussed in Thread: SN74LVC32A I have a follow up question for a third case: This is for using the SN74LVC32A, but I guess it has similar characteristics to the device in the subject. What are the implications for using this case? case 3.…
Part Number: SN74LVC32A This is Joong-hyeok Lee, DMSMS researcher of Leoinnovision.
Leoinnovision is the official EOL(End Of-Life)/obsolescence part manager of Korean Military (Army, Navy, Air force) and PLM agency of many defense industries (Hanwha,…
Part Number: SN74LVC32A Other Parts Discussed in Thread: SN74LVC1G3157 , Hello Team,
Can you provide the Tjmax of our SN74LVC32A and SN74LVC1G3157 for long time work spec to me, there is no this spec in our datasheets? thanks.
Regards,
Nanfang
Part Number: SN74LVC32A Hello team,
My customer use our SN74LVC32A, now they test the input signal and the Input transition rise and fall rate is 10ns/V, which is higher than 7ns/V(our spec), it is OK, any risk? thanks
Regards,
Nanfang
There is no such automotive-qualified device. You have to combine multiple OR gates; 3× 3 inputs (SN74HCS4075-Q1), or 4× 2 inputs (SN74LVC32A-Q1, SN74HCS32-Q1, SN74AHC32Q-Q1, SN74LV32A-Q1).
There are no open-drain buffers with an /OE input.
You can put OR gates (SN74LVC32A) in front of open-drain buffers (SN74LVC07A) to make the outputs Hi-Z when /OE is high.
This can be implemented with 3× SN74LVC32A, 1× SN74LVC08A, and 1× SN74LVC1G97. Is it worth it?
If you can change the input signals, it would be possible to use a shift register like the SN74HCS595.