Part Number: SN74LVC541A-Q1 Other Parts Discussed in Thread: SN74CB3Q3245 Hi there,
My customer used SN74CB3Q3245 for signal swtich. They are confused with 'Latch-up performance'. So could you give me an explanation about this function?
I can…
Part Number: SN74LVC541A Other Parts Discussed in Thread: SN74AHCT541 Is 5V ok to be applied to pin 20 Vcc of SN74LVC541APWR? The recommended is 3.3V, but I see the max rating is 6.5V. So does that mean 5V Vcc is ok? That means the output will be 5V with…
Part Number: SN74LVC541A Dear team,
Customer tested that when the voltage of Pin 6 >5.5V, this channel will be hurt and the output always low. I see from datasheet that the absolute voltage of Pin 6 should be 6.5V. And the fault rate is about 4/226=1…
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: SN74LVC541A Hi team,
My customer is using the SN74LVC8T245 and SN74LVC541A. Could you please help with the question below from the customer?
The customer is using the SN74LVC8T245 with VCCA=3.3V…
Rd is not needed at all. You need termination only at the receivers.
With a 2.5 V supply, HC outputs are much weaker; 32 mA will not be possible.
When you are changing the board anyway, why not use the DSLVDS1047, or at least the SN74LVC541A?
No; the inputs are always active. If the input signals can go inactive, then you have to add pull-up/-down resistors or use the SN74LVCH244A.
You might prefer the SN74LVC541A for easier board routing, but the variant with bus-hold inputs exists only with…
Part Number: SN74LVC541A Hi support team.
I received some inquiries regarding Fig 5 Icc vs frequency at P12 in datasheet from my customer.
1. Is it MHz as the unit of frequency on the horizontal axis?
2. Is the value of Icc for 1ch or the sum of all channels…
Part Number: SN74LVC541A Other Parts Discussed in Thread: SN74LVC540A , SN74LVC08A , SN74LVC1G97 Dear Team,
Here is Kevin from the Delta Taiwan team.
The customer is using 74LVC541 from Nexperia.
Do we have a similar device but the output will pull low when…
Part Number: SN74LVC541A Other Parts Discussed in Thread: SN74LVC125A , SN74LVC126A Is there a specification of the rise and fall time of the inputs of this part?
Regards Marc
Part Number: SN74LVC541A For SN74LVC541A VCC : 3.3V, output is enable properly
if my input pin voltage (at A1 Pin - A8 Pin) is 1.8V, what shall be the output voltage?