Part Number: SN74LVC541A-Q1 Dear TI experts,
Could you check the functional safety report of SN74LVC541AQPWRQ1?
I cannot find the document in TI.com
Best regards,
Chase
Part Number: SN74LVC541A-Q1 Tool/software: Hi team,
Do you have the FIT value based on SN29500 at 85C? I checked MTBF and FIT rate estimator on TI.com, but there is no information of what profile did the estimator use.
If you have already created…
Part Number: SN74LVC541A-Q1 Hi Team,
Please help confirm that considering that SN74LVC541A-Q1 uses three-state CMOS output, should the unused output pins be left floating?
Regards, Hailiang
Part Number: SN74LVC541A-Q1 Other Parts Discussed in Thread: SN74CB3Q3245 Hi there,
My customer used SN74CB3Q3245 for signal swtich. They are confused with 'Latch-up performance'. So could you give me an explanation about this function?
I can…
Hi Michael,
Thank you for responding.
Do we have latch-up information for SN74LVC541A-Q1 like the one for SN54LVC541A ?
Appreciate your help.
Thank you.
Regards,
Mark
Part Number: SN74HCS541-Q1 Other Parts Discussed in Thread: UCC23513 , SN74LVC541A-Q1 , SN74HCS541 , , SN74LVC541A We'd like to know what is the VOH and VOL @ Vcc=3.3V. in the datasheet d/s, it just specify the VOH at 4.5V and 6V. Could you also offer…
Please note that when going outside the recommended operating conditions, the electrical characteristics are no longer guaranteed, so 50 mA would be unlikely to work for your circuit.
There is no P2P part with 100 mA. You have to combine multiple outputs…
Part Number: SN74HC595 Other Parts Discussed in Thread: SN74LVC541A , TPIC6B595 Hi team,
We want to use SN74HC595 to drive seven-segment numerical tube LED as below.
Each moment, they will only drive one segment for 100us. But they need 20mA current…