Part Number: SN74LVC573A Hi,
We are using SN74LVC573ARGYR in various designs. We found a phenomena and we intend to check if issue is being familiar with such a scenario by TI / or cy customers.
In a specific design, one of the inputs (D6) is connected…
Part Number: SN74LVC573A-Q1 Dear team,
We are using this part ( SN74LVC573AQ1 ) in one of our projects,
1. We want to know if the latch output enable pins are left open and Latch enable is low, what will be the output state of the Latch - upon Power…
Part Number: SN74LVC573A Hi Team,
According to SN74LVC573APW datasheet, my customer has a concern about the temperature.
Operating free-air temperature: –40 to 85 °C
Op Temp: -40 to 125 °C
Is it a missing or Operating free-air temperature…
Part Number: SN74LVC573A Hello,
is the SN74LVC574ARGYR qualified for Ta -40°C to 125°C ?
On page 2 in the datasheet -40°C ..85°C is specified for VQFN20 package (this is the RGY type)
On abbendum page 2 the datasheet specifies -40°C to 125°C…
Part Number: SN74LVC573A Other Parts Discussed in Thread: SN74LVC574A Hi, Team,
My customer find there is some output issue for the SN74LVC573A. Could you help check it?
Issue: When output a low level voltage for the SN74LVC573A, there is some oscillation…
Part Number: SN74LVC573A hi dear supporting team,
what's the max junction temp of SN74LVC573APWR? there is no information in d/s. and from calculation, the max power consumption at 3.6V is only 0.036mW, is this correct? tks!
Part Number: SN74LVC573A Other Parts Discussed in Thread: SN74HCS573 , SN74LVT573 Tool/software: 標準ロジックIC573を使用して5Vから3Vに変換する場合、SN74LV573、SN74LVC573、SN74LVT573、SN74HCS573のどれを選択するのが最適ですか?
Hello Jerry,
Please refer to the following FAQ to calculate your output currents.
e2e.ti.com/.../742466
One key difference between the SN74LVC573A and SN74LVC373A is that the 573A has a flow through architecture. This means that 1D is in line…
SN74LVT573 , SN74LVC573A, SN74LVT373 , SN74LVC373A
If you need it clocked SN74LVT574 , SN74LVC574A, SN74LVT374 , SN74LVC374A
Thes will all have skews better than 1ns.
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage Translation FAQs - All-Time
How does a slow or floating input affect…