Part Number: SN74LVC8T245-EP Other Parts Discussed in Thread: SN74LVC8T245-Q1 Hello,
Could you help check and advise the difference between SN74LVC8T245-EP and SN74LVC8T245-Q1?
Except the operating temperature range, is there any other difference?
If the…
Part Number: SN74LVC8T245 Dear Specialists,
My customer is considering SN74LVC8T245 and has a question.
I would be grateful if you could advise.
---
Regarding SN74LVC8T245, the datasheet P.6 6.6 Electrical Characteristics doesn't described VOH/VOL when…
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: SN74LXC8T245 hi,
I encountered some problems when using SN74LVC8T245PW. When my board was just turned on and the MCU main program was not running, the output pin of SN74LVC8T245PW would have s…
Part Number: SN74LVC8T245 Dear Sirs
I'd like to know the capacitance value that can be directly connected to the output terminal of SN74LVC8T245.
According to the data sheet,the maximum charge/discharge current of the output is +/-50mA(continuous…
Part Number: SN74LVC8T245 For SN74LVC8T245, when the output voltage is fixed to high and when it is set to low which one saves power? Please tell me why.
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: SN74LXC8T245 Hi team, The DS has been revised and the following text added at the power supply recommendation section. >The recommendation is to first power-up the input supply rail to help avoid…
Part Number: SN74LVC8T245-EP Hi,
I'm trying to share SN74LVC8T245-EP across 1.8V/2.5V -> 3.3V conversion.
My application is similar to picture in Section 10.2 of the device datasheet. The direction is fixed portA (1.8V) to portB(3.3V).
But I also…
Part Number: SN74LVC8T245
Hi,
We are using the SN74LVC8T245DBR for the voltage level shift (for the 1.8v to 5v with the A to B operation ), Please explain more about this function. If we use it in our application, which is mentioned image below.
As per…
Part Number: SN74LVC8T245
Hi,
Greetings of the day,
We follow the A to B operation mode in this project.
But, We can't get the signal flow(Pulse) from PORT A INPUT (INPUT from the C6678's GPIO pin) to PORT B's OUTPUT.
What is the problem…
Part Number: SN74LVC8T245-Q1 I need decaps requirement for for both Vcca and Vccb power pins of SN74LVC8T245-Q1 8bit level translator when Vcca is 3.3V and Vccb is 1.8 V. I am level shifting 3.3 V signals to 1.8V signals.