Part Number: SN74LVCH16T245 HI,
One of my customer is asking about our SN74LVCH16T245
They are using a 5V output, that will drive a RC circuit (100kHz, 3.3nF) at 110kHz
Could you please comment on the device max output peak current?
The…
Part Number: SN74LVCH16T245 Other Parts Discussed in Thread: SN74LVCH16374A , SN74AXC8T245
Dear TI experts,
My customer considers SN74LVCH16T245 for their new product, and they have a question about data rate.
the condition that my customer want…
Part Number: SN74LVCH16T245 Hi,
For an LVTTL in and out buffer we are planning to use this device. Please confirm whether it is compatible with LVTTL input and output levels
Thanks
Part Number: SN74LVCH16T245 Other Parts Discussed in Thread: SN74LVC16T245 Hi Team,
A customer tested SN74LVCH16T245 in their project noticed that the Level translator output holds the previous state when logic input to the level translator is removed…
Part Number: SN74LVCH16T245 Other Parts Discussed in Thread: SN74LVC16T245 I have an existing design that uses the bus-hold '245 part as a level shifter. I would like to drive one of the inputs with an open drain driver but using a pullup resistor is…
Part Number: SN74LVCH16T245 The SN74LVCH16T245 which is a 16-Bit Dual-Supply Bus Transceiver, Configurable Voltage Translation, 3-State Outputs.
I have a hardware problem and I want to fix it. My preferred method is to change the VCCA 3.3V bus on my…
Part Number: SN74LVCH16T245
Hi sir/mam.,
I need to know the power consumption of the SN74LVCH16T245DGGR, SN74AVCH4T245PWR, SN74AVC4T774RSVR IC's. I have calculated the but I want to know whether calculation is correct or not. Kindly help me on this…
Part Number: SN74LVCH16T245 Is the channel to channel skew documented anywhere? We level translate 1.8V on VCCA to 3.3V on VCCB and our load is < 1" trace to 49.9ohm resistor, 50ohm transmission line < 6" to a 55LVDS31.
Part Number: SN74LVCH16T245 Hello,
I haven't seen anything about the effects of transient loss of a VCCA or VCCB power supply in the datasheet.
In our design, there may possibly be the loss of one of these voltages (3.3V and 1.8V) for a maximum time…