Hello,
In our board FPGA I/O lines are connected to the inputs of the 245 and the I/O voltage is set to 2.5V. The FPGA is not configured so I presume the interface pins between the FPGA and 245 must be tri-stated. The 245 might either be pulling up…
user4350686 - my feedback is below:
user4350686 said:
i am using SN74LVCH16T245 to translate 2V5(from FPGA-EVB) to 1V8(connect to our board), total 16bits used. i am not sure this component can support up to 130Mbps.(spec said it could)
I read…
Part Number: SN74LVCH16T245 Other Parts Discussed in Thread: ISO7640FM Hi,
I'm developing with SN74LVCH16T245 right now, to transfer 3.3V from/into 5V in my design, but I found the signals are interfered by the following circuits, so I want to replace…
Part Number: SN74LVCH16T245-EP Hello,
When we are simulating with SN74LVCH16T245-EP transceiver, and running for 100 MHz frequency, the result across 1K load with 1inch trace is as shown below,
Peak-to-Peak Voltage: 1.59 V
Max peak: 1.51…
rainbow,
Sorry for the delayed response.
For proper operation of the SN74LVCH16T245, /OE must be set to a valid Logic High or valid Logic Low at all times during device operation (as shown in the table below). It should never be left floating.
…
Other Parts Discussed in Thread: SN74LVCH16T245-EP What is the maximum acceptable Junction Temperature, Junction-to-Case Thermal Resistance (theta - JC) and
Junction-to-Ambient Thermal Resistance (theta - JA) for the device SN74LVCH16T245-EP ?
Other Parts Discussed in Thread: SN74LVCH16T245 DEARS.
Cio of SN74LVCH16T245 is mean?
Product variation is generated during production?
SN74LVCH16T245 variation is a value that can be generated during operation?
It can be changed due to the…
Part Number: SN74LVCH16T245-EP Hello,
Can you please provide the Junction-to-Board Thermal Resistance (Theta-JB) for the device CLVCH16T245MDGGREP ??
Regards,
Goutham
Other Parts Discussed in Thread: SN74LVC8T245 , SN74LVCH16T245 I need to convert I/O signals between a 5V ASIC and a 3.3V FPGA. I was planning to use the SN74LVC8T245 with VCCA = 3.3V and VCCB = +5V. The ASIC will tristate its I/O signals for lengthy…