Part Number: SN74LVCH16T245-EP Other Parts Discussed in Thread: SN74LVCH16T245 Tool/software: Hey team - can you help with the below?
The SN74LVCH16T245 has all inputs and outputs used, no pull-ups/pull-downs used at the input.
The voltage is translated…
Part Number: SN74LVCH16T245-EP Hi Team, Can we clarify the difference between CLVCH16T245MDGGREP and CLVCH16T245MDGVREP? From my initial checks it seems that the only difference is their SOP package variant - DGG and DGV. The SN74LVCH16T245-EP product pa…
Part Number: SN74LVCH16T245-EP I am looking to find the Temperature Cycle or Thermal Shock test setup for V62/09605-01XE (orderable device in SN74LVCH16T245-EP spec sheet)
Part Number: SN74LVCH16T245-EP Hello Guys,
Good day.
What is the debounce time on input "A" of the device sn74lvch16t245-ep?
i.e. Our customer is trying to understand what duration of glitches on the input signal will be filtered out by the…
Part Number: SN74LVCH16T245-EP Hi Team,
This is customer request can you please advise:
"
SN74LVCH16T245-EP level translator product of TI is being used in a design.
During tests, we detected a problem with this translator. VCCA and VCCB supplies…
Part Number: SN74LVCH16T245-EP Hi
I am using some SN74LVCH16T245-EP for level translating from 3.3V (port A) to 5V (Port B). It is indicated in the datasheet that the control signals (#OEn and DIRn) are related to VCCA which is 3.3V in my case. There is…
Part Number: SN74LVCH16T245-EP Other Parts Discussed in Thread: SN74LVCH16T245 , Hi, there.
I am using SN74LVCH16T245-EP in one of my project. Here I am driving 16 IO's of SN74LVCH16T245 from B port to A port. A port is referenced to 3.3V and B port…
Part Number: SN74LVCH16T245-EP I am interested in using this part, but for a space application. I have a couple of questions to this end:
- Is any radiation testing data available for this part?
- Is there a space grade version of this part in a ceramic…
Part Number: SN74LVCH16T245-EP Hello,
When we are simulating with SN74LVCH16T245-EP transceiver, and running for 100 MHz frequency, the result across 1K load with 1inch trace is as shown below,
Peak-to-Peak Voltage: 1.59 V
Max peak: 1.51 V
Min peak…