Part Number: SN74LVCH16T245-EP Hello,
When we are simulating with SN74LVCH16T245-EP transceiver, and running for 100 MHz frequency, the result across 1K load with 1inch trace is as shown below,
Peak-to-Peak Voltage: 1.59 V
Max peak: 1.51…
Other Parts Discussed in Thread: SN74LVCH16T245-EP , SN74LVCH16T245 Hello,
We require the IBIS model for the device SN74LVCH16T245-EP.. Can u tell how can I download IBIS model ..?? I searched in TI website . it shows tat IBIS model for the device SN74LVCH16T245…
Part Number: SN74LVCH16T245-EP Hello,
Can you please provide the Junction-to-Board Thermal Resistance (Theta-JB) for the device CLVCH16T245MDGGREP ??
Regards,
Goutham
Other Parts Discussed in Thread: SN74LVCH16T245-EP What is the maximum acceptable Junction Temperature, Junction-to-Case Thermal Resistance (theta - JC) and
Junction-to-Ambient Thermal Resistance (theta - JA) for the device SN74LVCH16T245-EP ?
Part Number: SN74AVCH16T245 Other Parts Discussed in Thread: SN74LVCH16T245-EP , SN74LVC16T245 , SN74AVC16T245 , Tool/software:
Component Ti : SN74AVCH16T245GR et SN74LVCH16T245-EP :
O n one of our designs we performed stress analysis on contations…
1. Testing is expensive; I guess there have been no customers for this so far.
2. 2× SN74AHC244-EP or SN74AHC245-EP in the TSSOP package has 2 × 6.5 mm × 6.4 mm; 2× SN74LVC8T245-EP in the VQFN package has 2 × 5.5 mm × 3.5 mm; SN74LVCH16T245-EP in the…
Apologies, I was looking at the SN74LVCH16T245-EP datasheet.
I think what I'm really trying to get at is what are the input/output power limits on the device? Do I use the type of supply current you mentioned to calculate input power or something else…
Other Parts Discussed in Thread: SN74LVCH16T245-EP Hi,
What is the maximum acceptable Junction Temperature, Junction-to-Case Thermal Resistance (theta - JC) and
Junction-to-Ambient Thermal Resistance (theta - JA) for the following devices
1) 74AVCH1T45DCKTG4…
Other Parts Discussed in Thread: LMZ31710 , LMZ31704 , SN74LVCH16T245-EP Hi,
We are using LMZ317 series power modules to generate required on board voltages. During PCB design, we are facing space limitations. Please suggest 1. Can two power modules…