Part Number: SN74LVT125 Other Parts Discussed in Thread: SN74LVTH125 , SN74AHCT125 , SN74LVC125A , SN74LV125A , SN74AHC125 Tool/software: Dear, Logic Support team. When I searched for the SN74LVT125 series, I found that both LVT and LVTH have a bus hold…
Part Number: SN74LVT125-Q1 Other Parts Discussed in Thread: SN74AC245-Q1 , SN74LVC125A-Q1 Tool/software: Hello, does TI have any quad channel buffers that can support a 4-wire JTAG interface (TDI, TDO, TCK, TMS)? Not sure there exists a part that can…
Part Number: SN74LVT125 Hi,
The App note says 'All newly developed bus-interface device inputs have a bus-hold circuit.'.
Is this only for AXC and AXCH?
The LVT already has a bus hold circuit. Is that of LVTH another newly designed circuit?
Is…
Part Number: SN74LVT125 Other Parts Discussed in Thread: SN74LVC125A Can I apply 100Mhz square wave signal input to SN74LVT125?
I have apply 100Mhz signal with no load it was giving Sinewave of 3.3v Around.
But when I connect 5mA load signal attenuate…
Part Number: SN74LVT125 I am Getting output voltage Range between 4v to 5v. And it also Goes in Negative Range.
And i have applied VCC 3.3V.
Input in Range of 3.3V to 4V.
I have attached the schematic and output Result.
My input in Range of…
Part Number: SN74LVT125 Other Parts Discussed in Thread: SN74LVTH125 Hi support team.
I received the following some questions from my customer.
1. Does this mean that pull-down / pull-up resistors are not recommended for both input (A) and output…
Part Number: SN74LVTH125 Other Parts Discussed in Thread: SN74LVT125 , Hi team,
Could you pleas share the difference between the SN74LVTH125 and SN74LVT125? Thanks.
Part Number: SN74LVT125-Q1 Other Parts Discussed in Thread: UCC21520 Hello,
I am adopting this device for the buffer placed between MCU and UCC21520.
According to the datasheet, the device is specified to have 128 mA and 32 mA for absolute maximum…