Part Number: SN74LVT16244B Hi
My customer is using SN74LVT16244B. Datasheet shows Vin range is -0.5V-7V. For customer Vin will be below -0.5V for about 10ns. Please help with below two questions. Thanks a lot!
1.What is Vin min value considering just existing…
Part Number: SN74LVT16244B Other Parts Discussed in Thread: SN74LVTH16244A Hi dear supporting team,
is there any pull up or pull down circuit at SN74LVT16244 input? tks a lot!
Part Number: SN74LVT16244B Other Parts Discussed in Thread: SN74LVTH16244A Hi
For SN74LVT16244b, what pull up value should use for input? When use 10kohm to pull up, output is low. But when use 2kohm to pull up, output is high. How to calculate the value…
Other Parts Discussed in Thread: SN74LVT16244B DEARS.
If there is capacity problem in SN74LVT16244B , while we open input pin which is not used in SN74LVT16244B .
Do we must connect input pin(not used input pin)to GND?
Thank you
Other Parts Discussed in Thread: SN74LVC2T45 , TXB0102 , TXS0102 Hi Shreyas,
My customer used SN74LVC2T45 as level shift in their system. However, they met the same problem as the input slew rate is too small and output start to ringing. they've tried…
Hello Emrys,
Thanks for the information, going back to this case:
Can you please explain how the reading of 40mV exist?
Additionaly, s omething with relatively low resistance (lower than the “large” 100 kOhm resistor we are using for a pull up). So what…
Part Number: SN74LVTH16244A Other Parts Discussed in Thread: SN74LVT16244B Hi team,
My customer is using the device SN74LVTH16244ADGG now. But the input Tr/Tf:113us/V, but the datasheet can only accept Tr/Tf:Max 10ns/V. Do we have some methods to do P2P…
Other Parts Discussed in Thread: SN74LVT16244B Hi,
I have about 40 single-ended signals (3.3V logic) that need to go from a Processor to an off-board unit. These signals need to go through a 20" (0.5meter) cable. The maximum frequencies of these signals…
Other Parts Discussed in Thread: SN74LVT16244B Hi
Iam currently driving the 16 to 20 LED's thru this buffer, controlling thru Micro-controller. Microcontroller GPIO pins are connected to below buffer and output of the buffer driving the LED's. the each…