Part Number: SN74LVTH16244A Hi Team,
You know our SN74LVTH16244A defines the max Δt/Δv should below 10ns/v. Pls see below datasheet screenshot.
But currently customer's slow input signal cannot meet this specification. What the risk is if the signal…
Part Number: SN74LVTH16244A Other Parts Discussed in Thread: SN74LVTH16245A , For the devices 16244/16245 I do not see a parameter "Continuous current through VCC or GND" in the datasheet. Is this specified?
Part Number: SN74LVTH16244A Hi,
Can you please advise for SN74LVTH16244ADGVR what is the max. absolute rating for the junction temp? Do you have a graph for MTBF vs. junction temp?
Thanks,
Hana
Part Number: SN74LVTH16244A Other Parts Discussed in Thread: SN74LVC162244A , SN74LVC16244A-Q1 Hi.
We want the SN74LVTH16244A but without the function
“Active bus-hold circuitry holds unused or undriven
inputs at a valid logic state. Use of pullup…
Part Number: SN74LVTH16244A Hello Guys,
Good day. One of our customer have a few inquiries with regards to SN74LVTH16244ADGG and SN74LVTH16244ADGGR. Aside from the suffix ‘R’ which is just a package carrier indicator, they want to know why the SN74LVTH16244ADGG…
Part Number: SN74LVTH16244A Hi team,
My customer is using two 16244 in the system( left side and right side). Whether we need to use the pull up resistors at right side when remove the left side board? Because the chip has the bus hold function, what…
Part Number: SN74LVTH16244A I have a customer who is trying to use the SN74LVTH16244A. He has the VCC pins tied to 3.3V. He has 5V TTL inputs and he's seeing outputs going to 4.7V, well above the 3.3V supply. Is this to be expected? He expects and wants…
Part Number: SN74LVTH16244A Hi there!
My customer received a reel of these parts with what we think are 2 different lot/date codes. Can you provide a decoder?
Thanks! Kara