Part Number: SN74LVTH241 Tool/software: Hi TI team,
I'm using some mux and buffer for JTAG application.
Need TI team to review the application in terms of correctness of part select, pull up/low resistor which concerning about active bus-hold feature…
Part Number: SN74LVTH241 Hi TI team.
I have tested using sn74lvth241pwr (buffer) in my application.
The problem is Input of buffer keeps the 'H' signal after a single pulse. What is reason input is not back to 'Low' when disappea single pulse.
The…
Part Number: SN74LVTH241 Hello all,
Can you provide the
Typical Power dissipation (Pd typ) & Maximum Power dissipation (Pd max) for the SN74LVTH241DWR device
or a formula to calculate it?
Thanks in advance.
The SN74LVT543 was released with the Bus Hold feature.
The name should have been LVTH543.
In 1997, we issued PCN 5287A informing customers of the name change with a redesign.
In 1999, we issued PCN 5322A notified customers of the nomenclature…