Part Number: SN74VMEH22501 Tool/software: Hi Everyone,
I need some clarification on below highlighted:
1. What should be voltage level at pin 42 and pin 31? what is the application of pin42 and pin31?
2. Why we used 1.5V in below image?
3…
Part Number: SN74VMEH22501 Other Parts Discussed in Thread: SN74HCS245-Q1 Please can you address a reference design making use of SN74VMEH22501?
Please can you address decoupling recommendation for this device?
Many thanks
Andrea
Part Number: SN74ABT245B Other Parts Discussed in Thread: SN74VMEH22501 , SN74AHCT245 , SN74LVC245A Tool/software: Hi Folks,
We are planning to use SN74ABT245B as a transceiver in new VME design.
Below are details of VME board which we are going to…
Part Number: SN74VMEH22501 I was going to use the SN74VMEH22501 in a new design.
I noticed in the simulation that this part causes a little bit of ringing but if I add a 10 ohm series termination on the vme bus side of the part, it reduces it quite…
Part Number: SN74VMEH22501 We are using SN74VMEH22501 buffer in a project of ours
The master of the bus is a CPU board, and in the backplane 6 I/O slots are available, and (in the example below) only two slots are populated with an I/O board
In…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74VMEH22501 Dear Team,
Can you please share me the power dissipation calculation detail of SN74LVC16T245 and SN74VMEH22501.
Regards,
Prasanna G
Hello,
please consider ringing issue closed; we are experiencing a very blocking issue on the buffer when we want to perform EFT burst tests.
We are assisting at the following problem:
focusing on the *nCS0 signal (a chip select), in normal operation…
Other Parts Discussed in Thread: SN74VMEH22501 Hi,
I am using VME buffers with part number SN74VMEH22501 for interfacing VME bus to kintex 7 FPGA. Please let me know if there is any standard desing or layout guidelines to be followed for implementing…
Hi Lilian,
We don't really have anything that fits those requirements. Most of our devices with level 3 isolation are in the GTL/GTLP family and those are app specific devices. Here's a device you can take a look at that may work for them: SN74VME…