Part Number: SN75LBC180 Other Parts Discussed in Thread: SN751178 When SN75LBC180 connect with SN751178 for below circuit, waveform was oscillation, please let me know about three points below;
①When SN751178 Tx set disable, waveform was occur large…
Part Number: SN751178 Hi,
Customer is using SN75118N.
Differential input voltage sensitivity: The output is undefined at -200 mV <Vid <+ 200 mV.
The customer sets up a fail-safe circuit and fixes it to the "L" level when it is undefined.
Below…
Other Parts Discussed in Thread: SN751178 Hi Team, Is there absolute maximum ratings of appling external voltage for output pin? My customer wants to know if applying 5V to 1Y(14 pin) or 1Z(13 pin) could damage the device. I heard he mistaked to apply…
Other Parts Discussed in Thread: SN751178 Hi all, Would you mind if we ask SN751178? How much is the θjc? We could not find it on the datasheet. If you have the reference data, could you give us it? Kind regards, Hirotaka Matsumoto
Other Parts Discussed in Thread: SN751178 , SN75117
Hi Everybody!
I have a question about Internal "Fail Safe function" of SN751178 (RS485 Driver & Receiver).
I found Data Sheet (Page 1 ) that described "internal Fail Safe function" .
"Fail-safe…
Other Parts Discussed in Thread: SN751178 Dear Sirs,
My customer asked us about absolute maximum rating(IOH) in the receiver circuit of SN751178.
In the Receiver circuit,
The maximum value of the recommended current of High-level output current…
Part Number: SN65C1168E Other Parts Discussed in Thread: SN65C1168 , SN751178 , THVD1500 Tool/software: Hi all,
To replace the HD29051FP used as the RS-422 driver/receiver
We are considering using the SN65C1168E.
We replaced the SN65C1168E in the…
Part Number: SN65HVD30 Other Parts Discussed in Thread: THVD1451 , SN75LBC179 , THVD1512 , SN751178 Tool/software: Hi Team,
I would like to know the maximum operating current and standby current of the SN65HVD30DRG4. I couldn't find clear specifications…
Hey Dan,
LM120K-5.0/883 is indeed obsolete. I've attached the PDN.
We don't have an exact P2P replacement so I'd recommend the UA79 series as the closest alternatives.
~ Aaron
PDN 200824.pdf