Part Number: SN75ALS1178 Other Parts Discussed in Thread: THVD2450 , ESDS552 Hello,
I would like to ask about the overvoltage robustness of the SN75ALS1178NSR driver output pins.
The datasheet specifies the Absolute Maximum Ratings as: Vo = -9V to…
Part Number: SN75ALS1178 Tool/software: Hi TI Team,
Our customer requested the ESD please help to provide it.
Material name : SN75ALS1178NSR
Best regards,
Takako Fujiya/TED
Part Number: SN75ALS1178 Hi All,
I have a question about SN75ALS1178.
What are the lower limits of absolute maximum ratings for the DE pins (pin 4, pin 12) and driver input pins (pin 9, pin 15)? Only the upper limit values are listed in the datasheet…
Part Number: SN75ALS1177 Other Parts Discussed in Thread: SN75ALS1178 , , SN65C1168E , SN75C1168 , SN65C1168 Dear Specialists,
My customer is evaluating SN75ALS1177NS as a replacement for SN75ALS1178.
They have a question about current consumption…
Part Number: SN75ALS1178 Other Parts Discussed in Thread: THVD1451 , THVD1424 , SN65HVD70 , Hello,
I am using this transceiver to send signals between a 3.3V microcontroller to a 5V differential bus.
If I provide 5V to VCC and +/-5V signals to the…
Part Number: SN75ALS1177 Other Parts Discussed in Thread: SN75ALS1178 , HI Sir:
I want to confirm the below question
Does the SN75ALS1177 or the SN75ALS1178 include two transceivers and they compatible with RS422??
Thanks
Best Regards
Part Number: SN75ALS1178 Dear Specialists,
My customer is evaluating SN75ALS1178NSR(SO Package) and SN75ALS1178N(DIP package) .
They have questions, I would be grateful if you could advise.
---
Since SN75ALS1178NSR (SO Package) was not available…
Part Number: SN75ALS1178 Tool/software: What is the minimum operating voltage for SN74ALS1178? We understand the recommended operating voltage. (5V±0.25V)