Hi HK,
I was able to locate the top marking for devices from FMX. It looks like it matches what I see in our system.
There was a redesign of the die which may have impacted the top marking.
AM26C31 PCN20240328001.1.pdf
-Bobby
Other Parts Discussed in Thread: SN75ALS191 Hello! I have a question about non-standard use of SN75ALS191 and similar RS422 line drivers from TI: 1). Is it legal if both differential outputs are AC-coupled ? 2). Is it legal if both differential outputs…
Hello, Don!
Please then comment on this information from DIX4192 datasheet ( page 31 ):
"The SN75ALS191 dual line driver is especially useful in applications where simultaneous 75 Ohm and 110 Ohm line interfaces are required." ( page 31 ).
This…
Hello, I would suggest them to go through the data sheet and see the function of any un used pins ( most of these are OUTPUT pins). If it is an output or monitor pin ( like LOCK, RDY, TX+, TX- and etc ) they can just leave them float and most of the time…