Part Number: SN75DP126 Dear Sir,
Customer met some question while they implement firmware into their BIOS.
As customer feedback, there is no problem to write AEQ registers, but after write data into DPCD register and read back, all they can get is "0…
Part Number: SN75DP126 Dears,
Attached is the eye diagram of customer SI testing.
It seems the quality is not good to pass the test.
Is there any suggestion to pass the SI testing?
Thanks.
Part Number: SN75DP126 Hi,
From Fig 26 in datasheet, I understand that I2C_CTL_EN should be High to enter DP126 to compliance test mode. Then is it necessary to set I2C_CTL_EN to Between VIL and VIH or High for HDMI complicance testing? In other words, can…
Part Number: SN75DP126 Dear support,
The SN75DP126 device should provides the status of the Hot Plug Detect sink (HPD_SNK input) from a monitor to the digital controller (HPD_SRC output).
On a specific printed board assembly, one device is faulty responding…
Part Number: SN75DP126 Hi,
Now my customer is considering to use SN75DP126 for Skylake or Kabylake platform. Then they hope to refer the reference schematic and pin connection if you have. Can you share any document if you have? Please find my contact…
Hi Team,
One of my customers is really interested in SN75DP126 and would like to have its EVM user guide with the reference schematic. Is is possible to send those information to my email? Thanks for your support.
Leroy Song
Other Parts Discussed in Thread: SN75DP126 Hi Sirs,
Sorry to bother you.
We have use SN75DP126, one thing need to clarify
If only one signal plug in, TI IC can auto detect and output screen to monitor? Or we need adjust IC GPIO high or low to control IC…
Hi all,
This chip is connected to a xilinx FPGA which I am going to implement my IP core. My problems are,
1. To use the HDMI output do we have to input TMDS signals to the chip?
2. Does this IC have internal DP-to-TMDS converter ?
Thank you
Other Parts Discussed in Thread: SN75DP126 , SN75DP130 Hello,
I have a question, I have been searching for the right product the last few days and not sure if the above are the right ones.
I want to use a Displayport connector and connect this one to one…