Part Number: SN75DP130 Tool/software: Hi Teams,
Is there a corresponding SDK available for SN75DP130?
The customer followed the instruction sequence for writing DPCD in the reference manual, but all read values were 0. So he's not sure if he was writing…
Part Number: SN75DP130 Other Parts Discussed in Thread: DP130SSEVM Could you please share the OrCAD reference schematic and PCB data for the DP130SSEVM?
Part Number: SN75DP130 Tool/software: Dear Team,
Could you please tell me the correct package oytline for SN75DP130?
In datasheet, there are 2 type package outlines as page49-51 and page 52-54.
They differ in the size of the thermal putt.
Best…
Part Number: SN75DP130 Hello Please refer to Section 7.3- Recommended Operating Conditions
For V IH and V IL,
V IH has a range of 1.9V - 3.6V, but the nom RST pin voltage is listed as 0.75V, which is not in the 1.9 - 3.6V range whatsoever.
V…
Part Number: SN75DP130
Tool/software:
Dear Technical Support Team,
I'd like to lane swap.
For example,
Connect the source side LANE3± to the IN0± pins of the SN75DP130, and connect the OUT0± to the LANE3± on the sink side (DP connector).
…
Part Number: SN75DP130 Hi TI,
The architecture of our project eDP re-driver design is "DP only Configuration with AUX Pass Through" The problem currently encountered is that some machines will have intermittent images when the temperature is 80 degrees…
Part Number: SN75DP130 Tool/software: Hello experts
Hope this finds you well.
I am trying to change the SCL_CTL and SDA_CTL pins I2C for SN75DP130SSRGZ.
We think: If you change bit 7 of Offset 05h from 0 to 1 and change bit 4:3 value of Offset 15h…
Part Number: SN75DP130 Tool/software: Hi alll,
Regarding the equalizer, If the AEQ_L0_LANE0_SET setting in the data sheet is changed as follows, would it be possible to provide the equalizer transfer function parameters,like pole, zero and gain?
…
Part Number: SN75DP130 Tool/software: Dear , support team. Q1. Conditions for transition to Output Disable Mode. I understand that there are two conditions for transition to Output Disable Mode.
First. When a Squelch event occurs in the video signal…
Part Number: SN75DP130 Other Parts Discussed in Thread: TDP142 Tool/software: Dear, Interface Support team. Our customers have used SN75DP130. We would like to use SN75DP130 as a display SINK driver. There is a Simplified Schematic on the cover of the…