Part Number: SN75LV4737A Hello
The data sheet states that C2 is not used in a 5V operating circuit.
If C2 is connected,what kind of problems occur?
Best regards.
Part Number: SN75LV4737A Other Parts Discussed in Thread: SN74LVC1G34 Hello
Please tell me the maximum sink current when the receiver output (ROUT) is low.
If it can sink a current of 10mA, what is the maximum output voltage at that time?
Best regar…
Part Number: TUSB3410 Other Parts Discussed in Thread: SN75LV4737A , GD75232 what is the function of SN75LV4737A at TUSB3410 EVM ?
is it a must add in the EVM design for SN75LV4737A if we have other RS232 transceiver such as GD75232 ?
Part Number: SN75LV4737A Dear Specialists,
My customer is considering SN75LV4737A and has a question.
Could you please advise?
---
According to the datasheet, the external cap is recommended >0.1uF.
Are these possible to use 0.47uF?
What is the maximum…
Part Number: SN75LV4737A Hi,TI,
I'd like to know the spec of receiver input current ?
I try to recommed ths device in order to replace DS14C335. SD14C335 has the spec.
Part Number: SN75LV4737A hi,
One of my customer old design is using DS14C335MSA, TI has suggest to replace it with SN75LV4737ADBR. My customer has follow the advice but now they are facing lost link issue. Note this is just the suspect, below is the portion…
Part Number: TUSB3410 Other Parts Discussed in Thread: SN75LV4737A Hello,
I’m working on a reference design with a third-party USB-to-UART bridge that I would like to replace with a TUSB3410. In the datasheet, I saw this diagram which I wanted some…
Other Parts Discussed in Thread: SN75LV4737A , TUSB3410 Hi Lady & Gent, Can you help me to identify about TUSB3410? Can I remove SN75LV4737A if I only use SIN and SOUT for data transfer ? Thanks ! David
Hi Jeff,
Correct, a line driver for RS-232 side should be used. You can also look at SN75LV4737A (recommended) for this. This device also has internal ESD protection.