Part Number: SN75LVCP600 Hi all,
is it okay to have the signal connected with inverted polarity like this?
Input:
RX- (Pin3) = SATA_P_IN
RX+ (Pin2) = SATA_N_IN
Output:
TX- (Pin6) = SATA_P_OUT
TX+ (Pin7) = SATA_N_OUT
There any concerns on the OOP or…
Part Number: SN75LVCP600S Hi
In the Pin functions table the description for Control Pins EQ, DE, MODE & SQ_TH says internally tied to GND but in section 9.2.2 Detailed Design Procedure it says for low level, use 47-kΩ pulldown.
Which is correct…
Part Number: SN75LVCP600S Are you sure that this ic can be used as a sata 3 repeater?
I believe that it is available with a SATA3.0(6.0Gb/s) Repeater.
At this point,
1. the TX signal from the CPU enters LVCP 600 S.
2. This signal is confirmed from LVCP…
Other Parts Discussed in Thread: SN75LVCP600S Hi,
We have some questions about SN75LVCP600S waveforms during OOB, could you please help to explain the behaviors? Thanks for your support!
Please find the system diagram and the test points at TX below…
Hi,
We have some questions about SN75LVCP600S waveforms during OOB, could you please help to explain the behaviors? Thanks for your support!
Please find the system diagram and the test points at TX below, ( TP3 in Green is Input and TP5 in Yellow is output )
…
Other Parts Discussed in Thread: SN75LVCP600 Hi Sir
I have four questions about SN75LVCP600 as followings.
For the V(d iff Rx) spec min 120mV, the eye opening is defined after/with equalizing(EQ) in receiver or not?
Our simulation channel was using Keysight…
Part Number: SN75LVCP600S Support Path: /Other topics/Design techniques and how-to guides/ Hi,
I would like to know if AC coupling capacitors are needed between SATA components on same board with good ground plane?
My exemple is the use of repeaters…
Other Parts Discussed in Thread: SN75LVCP600 , SN75LVCP601 , SN75LVCP600S Hi all.
Is there the SN75LVCP600 IBIS Model available? If yes, may I get it?
Many thanks.
Other Parts Discussed in Thread: SN75LVCP600S , SN65LVCP1414 Hello.
Does the SN75LVCP600S use for general purpose high speed interface?
(not SATA/SAS)
Thank you.
Best Regards,
H.Fujikawa