Part Number: SN75LVDS82 Hi all Would you mind if we ask SN75LVDS82? <Question1> About LVDSGND, PLLGND and GND, is it possible to connect together? Or, do these GND pins have to be separeted? <Question2> If we have some unuse output pin(DXX), is it…
Hi Sheree,
Please see the SN75LVDS82 (receiver) and SN75LVDS83A (transmitter).
Note that some of the specs are slightly different, so please be sure to verify with your system parameters.
Thanks,
Kate
Other Parts Discussed in Thread: SN75LVDS82 , SN65LVDS822 Hi,
In my application I intend on the transmit being powered all the time, but the display has the ability to shut off, as does the flatlink receiver(SN75LVDS82 or SN65LVDS822) to save power. I’m…
Part Number: SN65LVDS86A Other Parts Discussed in Thread: SN75LVDS82 , Hi,
Is there have SN65LVDS86A reference design can provide to me?
My customer want to change LVDS solution from SN75LVDS82 to SN65LVDS86A,
They wants to know there have big change and reference…
If you are running at the lower pixel frequency, then yes, I would recommend the SN65LVDS94. Of course the SN75LVDS82 has a higher upper end frequency, so it depends on the pixel clock range you need to support. The above example is a relatively low pixel…
Other Parts Discussed in Thread: SN75LVDS82 Hi,
I am using the Flat link Deserializer SN75LVDS82.
I just wanted to clarify one point : are parrallel RGB outputs in high-Z state when nSHTDN input is active ? I would say so considering the "FUNCTIONNAL…
Other Parts Discussed in Thread: SN75LVDS82 Hello TI,
In this E2E support forum I exactly found my current question. I'm looking for a DSI to 8-bit parallel RGB conversion. In 2016 you suggested to implement a 2-chip solution SN65DSI85 + SN75LVDS8…
Hi Adrian,
What is the minimum resolution that you want to support? Please note that the resolution determines the clock frequency, and these parts have minimum/maximum supported clock frequencies. For the SN65DSI83, the minimum supported frequency is…
Part Number: DS90CF386 Other Parts Discussed in Thread: TFP410 , SN75LVDS82 , Hello
We are planning to implement a LVDS to DVI Interface. The plan is to prallelise the LVDS signals and send it trough the TFP410.
Now I'm looking for the right device to make…