Part Number: SN75LVDS83A Other Parts Discussed in Thread: SN75LVDS83B , SN65LVDS93A , SN65LVDS93B Hi,
We are considering a circuit to control an LCD, and are looking for an IC that can convert parallel RGB signals to LVDS. I would like to know the differences…
Part Number: SN75LVDS83A Other Parts Discussed in Thread: DS90C385A Hi, support team
Can SN75LVDS83A and DS90C385AMT replace each other? If can't, what is the different between them?
Thanks so much.
Best regards, Yuki
Part Number: SN75LVDS83A Other Parts Discussed in Thread: SN75LVDS83 , SN75LVDS83B
Hi Team, Is there IBIS model for SN75LVDS83A? Is it same IBIS model of SN75LVDS83(NRND)? http://www.ti.com/product/SN75LVDS83/toolssoftware Best Regards, Yaita
Part Number: SN75LVDS83A
Hi Team, I would like to ask two questions in datasheet. - Pin Functions table 1) There is no 33, 35, 36 pins in Pin Functions table. Should we consider 33, 35, 36 pin are all GND? 2) Pin Functions table shows 23 pin is GND however…
Part Number: SN75LVDS83A Hi Expert,
We are having a problem when connecting SN75LVDS83A to FPGA.
As shown in below capture, if SN75LVDS83A is connected to FPGA with CLKIN & D4. For CLKIN, distortion is found(Green waveform). However, the waveform on D4…
Part Number: SN75LVDS83A Hi
Pls advise should i use any TVS/ESD array to the o/p of SN75LVDS83A while connecting to LCD panel.
Do i need to place ESD array in all 4 differential o/p & clock o/p.
Part Number: DS90C383B Other Parts Discussed in Thread: SN75LVDS83B , SN75LVDS83A , DS90CF383B , Team,
-could you please clarify what are the differences between DS90 C 383B and DS90 CF 383B? -Also all 4 devices (SN75LVDS83A, SN75LVDS83B, DS90C383B, DS90CF383B…
Hi Sheree,
Please see the SN75LVDS82 (receiver) and SN75LVDS83A (transmitter).
Note that some of the specs are slightly different, so please be sure to verify with your system parameters.
Thanks,
Kate
Other Parts Discussed in Thread: SN75LVDS83A , SN75LVDS82 Hi Team,
My customer want to use SN75LVDS83a, but their system clock only 7MHz.
Can they just connect their system clock 7MHz into parallel data in (D0-D23) and use external 14MHz for CLKIN?
Thanks…