Part Number: SN75LVDS83B Other Parts Discussed in Thread: DS90CR287 I am looking for a Camera Link transmitter that will accept 1.8V logic on its input side. The DS90CR287 looks like the standard part to use other than the 3.3V-only inputs. I think SN75LVDS83B…
Part Number: SN75LVDS83B Hi,
Could you please recommend a chip which supports RGB16bit or RGB565 to 4 Lane LVDS? Does the SN75LVDS83B support this function? The LVDS signal outputs to LCD.
Thanks.
Kevin Xiong
Part Number: SN75LVDS83B Hi Team,
My customer is using the SN75LVDS83B for the RGB - LVDS solution.
And they're using the FORMAT 2 of the 24-bpp LCD display mode.
I checked the wire connecting is all right but don't find any instruction on how to…
Part Number: SN75LVDS83B Other Parts Discussed in Thread: AM3354 Dear Sirs,
We choose the TI AM3354 which connect to SN75LVDS83B to implement 24-Bit Color Host to 24-Bit LCD Panel Application.
After I read the datasheet of SN75LVDS83B, the page 28, Layout…
Part Number: SN75LVDS83B Other Parts Discussed in Thread: AM5728 Hi Team,
My customer accidentally hard wired the SN75LVDS83B to the AM5728 on their first batch of boards to JEIDA-24, but their display only support VESA-24.
Is there a way to re-map the…
Part Number: SN75LVDS83B
Hi,
We are using SN75LVDS83B to convert RGB (18 bits CPU) to a 10.1 display LVDS (24 bits) display.
We facing problems with the image. The colors is not good and there is a lot of noises either.
The image below is the linux boot…
Hi Antonio, To answer your questions,
- Do you have other similar device which can work at 1.8V LVCMOS levels and it is compatible with the serializer DS90CR217?
I will need to check this and get back to you.
- Do you think that the solution based on level…
Part Number: SN75LVDS83B Hi, I am looking for a serializer for a TFT Display with integrated LVDS deserializer. It should convert RGB 3 x 8-Bit to R, G, B signals and Clock.Supply Voltage is 3.3V, Pixelclock 18 MHz. Is the SN75LVDS83B suited for the application…