Please download the CSL package for C6713 which has CSL based examples for this SOC.
http://www.ti.com/tool/sprc090
We also provide board support library for this device here:
processors.wiki.ti.com/.../C6713DSK_in_CCSv5 (USe the Direct link for BSL…
Tool/software: Code Composer Studio Hello,
I got the DSP Starter Kit (DSK) for the TMS320C6713 board. There's the CCSv3 version included with all the necessary board specific content (C6000 CSL, CGT, DSP/BIOS,...). Since I have to run it on a Windows…
Hi Pradeep, If you are intending to use the ADS1282's FIR filter at 2 kSPS and 4 kSPS, then you'll need to supply the ADC with a 4.096 MHz clock, otherwise with a 2.048 MHz clock you'd need to program the ADC for twice the nominal data rate.…
Dear Souhir,
Please download and install the CSL package for C6713.
EDMA example location in CSL package:
C:\ti\C6xCSL\examples\c6000\dsk6713\csl\edma\edma1
Download:
http://www.ti.com/tool/sprc090
Hi,
Thanks for your post.
Yes, it can be used with Windows 7/8/10.
Please find the DSP Integration Workshop materials from below link which would help you better to understand C6x1x
http://processors.wiki.ti.com/index.php/TMS320C6x1x_DSP_Integration_…
Dear Chung,
Sorry for the delay in response since you might have posted in different E2E forum.
Also we don't have exact ADC example code but we do have audio McASP audio support which is useful when you work with ADC.
You can get those McASP related…
Hi Christian,
Thanks for your post.
I think, you could download c6x CSL which provides an API for configuring and controlling the DSP on-chip peripherals as below:
http://www.ti.com/tool/SPRC090
After downloading sprc090, please see 'Readme.txt" and Releasenote…
Hi,
The latest CSL can be downloaded here:
http://focus.ti.com/docs/toolsw/folders/print/sprc090.html
The 6713 CSL EDMA examples included in the above should be very similar for DSK6416 . One key thing you would need to change is in the build options…