Part Number: TMS320C5535 I have executed the programmer_C5535_eZdsp.out included in the C55XCSL-LOWPOWER following the steps below, but it does not seem to be working. Could you please confirm if my usage is correct?
In Code Composer Studio Version…
Part Number: TMS320VC5502 Other Parts Discussed in Thread: SPRC133 I'm working to setup a build environment in Code Composer Studio v12.5 for the TMS320VC5502 and then importing a v2.0 project into the v12.5 environment.
During custom installation,…
Part Number: TMS320C5505 Other Parts Discussed in Thread: SPRC133 Hello,
How to create a dummy section in the linker file?. I would like to create the output file without allocating the memory or filling the data in the DUMMY section of the output file…
Okutsu-san,
It looks like the CSL comes separately from this package:
https://www.ti.com/tool/SPRC133
The BSL looks like it comes from a 3rd party Spectrum Digital:
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/327265…
Hi Guntupalli,
You will need to download the SPRC133,
C55XCSL-LOWPOWER — TMS320C55x Chip Support Library for C5504/05, C5514/15/17 and C5535/45 devices from
SPRC133 Driver or library | TI.com
and the dependencies:
Release 3.08.01 Dependencies…
Hi Jun Ting,
You can download the C55x CSL 1.0.0 from https://dr-download.ti.com/software-development/driver-or-library/MD-0MVQS9HBZ7/01.00.00.00/sprc133.zip
C5502 Examples are at C:\ti\C55xxCSL\examples\c5502\csl.
Best regards,
Ming
Hi Matteo,
If you download and install the C55XCSL-LOWPOWER CSL 03.08.01 from SPRC133 Driver or library | TI.com , there is an example of I2C DMA in
c55_csl_3.08.01\ccs_v6.x_examples\i2c\csl_I2C_DMA_example
Best regards,
Ming
Hi Kishor,
You can download the C55XCSL-LOWPOWER 03.08.01 from SPRC133 Driver or library | TI.com . Install it at C:\ti, you will get the files I mentioned in previous post.
Best regards,
Ming
HI Kenji,
If you download and install the C55XCSL-LOWPOWER from SPRC133 Driver or library | TI.com and the pre-built programmer_C5535_eZdsp.out for C5535 will be at
C:\ti\c55_lp\c55_csl_3.08.01\utilities\Programmer\c5535. Load and run it on C5535…