Hello
Which exact signal(pin) do you expect to be de-asserted?
If you want to deassert POWER_LD or UCD_LATE_PG signal, you have to include rail2(3V3) and rail3(1V8) into the logic.
If you expect short 3V3 and 1V8 to turn off other power, please…
Hello,
I have some trouble to build the DVSDK 2 for the DM6467 EVM. My compiler is : gcc arm-2008q1 from code sourcery (gcc version 4.2.3 - Sourcery G++ Lite 2008q1-126)
I succesfully compiled : Montavista linux kernel 2.6.18 and a part of the DVSDK…
Hello Aneesh,
Please find attached Mathcad and excel sheets I used to design the PMP8740.
You should take into account though that all files refer to revision A of the boards, while all of them have been fine tuned until revision D, so you may expect…
Hi John,
Thanks for replying!
Yes we have not used current transformer or opamp. Voltage across shunt resistor is directly given to CSA and CSB pin for current sensing. I have attached Excel calculator again with schematic as shown below. I have…
Hello
Please see my comments
#1. slave fault shutdown and sequencer off dependences are two irrelevant. it is application's responsibility to set these to ensure dependencies are met.
Since rail#5 has turn off dependencies on rail6/7 you have to…
Part Number: DAC38RF82 Other Parts Discussed in Thread: LMX2820 , , LMK04832 , ADC12J4000 Tool/software: We had a board working with LMK04832 and LMX2820 for clocking, one DAC38RF82 and one ADC12J4000. Some changes where made to clocking and a new board…
Part Number: TMS320C6410 Tool/software: Code Composer Studio Hi
I'm getting below message when I run the simulation.
"TMS320C64X+_0: Warning: The application is using 64 MB of DSP memory. Verify application memory usage. To increase the supported…
Other Parts Discussed in Thread: MIDAS Hi, I'm chul.
I have configuration error at MIDAS Ultrasound v2.0 Demo step QT Libraries setup.
First, I try follow website as blow.
Qt Libraries
1. Download the Qt libraries 4.6.2 for embedded…
Hi Steven,
Currently we were upgrading our wiki pages, thats why they are not reachable. The PDF version of the link is attached below,
Configuring Interrupts on Keystone.pdf
Thanks,
Rajarajan U
Hi Wayne,
There's an app note that discusses this that appears to have been removed. I'm attaching it here. Please take a look and let us know if you have any questions!
Synchronizing Multiple ADC3101.pdf
Best,
Zak