Part Number: SW-DK-TM4C129X Hello!
I have an Graphic LCD display application to be implemented. So I am using DK-TM4C129x for the same. I wanted to display various input and output data coming from my external devices that will be connected to the development…
Part Number: SW-DK-TM4C123G Other Parts Discussed in Thread: TM4C123GH6PGE This concerns programming the ADC.
First the basics:
CCS version: 7.3.0.00019
PC OS: Win10
TI Code base: TivaWare_C_Series-2.1.4.178
Data sheet: Tiva™ TM4C123GH6PGE Microcontroller…
Part Number: SW-DK-TM4C129X Other Parts Discussed in Thread: EK-TM4C1294XL , EK-TM4C123GXL
Using the TI board above to initialise a second board. I have gone through and programmed multiple of the second board using a JTAG link but on the 5th board…
Part Number: SW-DK-TM4C129X Hi TI-team,
I would like to use the lwIP TCP/IP stack to implement a Modbus TCP/IP protocol on a TM4C129X or MSP432 microcontroller.
I have a DK-TM4C129X development board and went through some examples like the "Ethernet…
Part Number: DK-TM4C123G hello ,
I was able to run the program which were given in the tivaware examples in DK-TM4C123GH6PGE . But while creating new project for graphics example i am getting
#1965 cannot open source file "drivers/cfal96x64x16.h…
Part Number: DK-TM4C123G Hi Team
I have DK-TM4C123G Rev A0.
Is it the latest version? I couldn’t find the information for it.
Is there any limitation to use this?
Thanks and Best regards,
Kuerbis
Part Number: DK-TM4C123G Other Parts Discussed in Thread: EK-TM4C123GXL Does anyone know why TI disgnated the DK-TM4C123G obsolete? I think it is a great development kit. One of the best for CAN development. Is there a newer kit in the TM4C123G series…
Part Number: DK-TM4C123G Hi,
I am trying to set up CAN demo on two DK-TM4C123G demo boards. I have added two 120ohm resistors to both sides. The data did send from TX side and I can measure it on CAN wire. I also measure the signal between CAN transceiver…
Part Number: TM4C123GH6PGE Other Parts Discussed in Thread: TM4C123GH6PM ,
Q1> In the figure ③, “pcm xxxx 16bit xxxx. wav ”file cannot be played.
Send me a wav file that can be played ?
Q2> I use the audio conversion program of NCH Sotfware Company…
Part Number: DK-TM4C123G Other Parts Discussed in Thread: EK-TM4C123GXL Dear team:
Do you have another development kit for CAN protocol similar to the following?: TM4C123G USB CAN Development Kit DK-TM4C123G
Best regards