Part Number: SW-EK-TM4C1294XL Other Parts Discussed in Thread: EK-TM4C1294XL I am attempting to run the example projects provided for the EK-TM4C1294XL dev kit however whenever I click "import" in Resource Explorer for a project it pops-up saying I must…
Part Number: SW-EK-TM4C123GXL Other Parts Discussed in Thread: EK-TM4C123GXL Hi everyone,
I am trying to create an application where the TIVA is configured as USB device which communicates downstream through serial port.
I am already tested with success…
Part Number: SW-EK-TM4C129EXL Other Parts Discussed in Thread: EK-TM4C1294XL I'm having trouble determining which pins and software controls will to properly do bi-mode SSI.
The frame sync pin function is not fully clear.
My design uses two shift loops…
Part Number: SW-EK-TM4C129EXL Other Parts Discussed in Thread: UNIFLASH , EK-TM4C1294XL Hi,
I am using the boot_serial example from the SW-EK-TM4C129EXL and have followed the procedure outlined in the document Getting Started with TivaWare for C Series…
Part Number: SW-EK-TM4C1294XL Other Parts Discussed in Thread: EK-TM4C1294XL Dear Sirs
I'm using the EK-TM4C1294XL as a master unit to communicate with a embedded pressure sensor that I'm developing. To get started, I'm using the example projec…
Part Number: SW-EK-TM4C123GXL
I've an interrupt clocked at 100kHz - so need it to be as efficient (e.g. minimum clocks) as possible.
So I changing the calls to libraries, to direct writes to the memory mapped registers. This basically just removes…
Part Number: SW-EK-TM4C129EXL Other Parts Discussed in Thread: EK-TM4C129EXL , TM4C129ENCPDT Hi, I am trying to use freeRTOS on EK-TM4C129EXL. I have followed this older tutorial and tried to build the project, but I get the following errors:
Building target…
Part Number: SW-EK-TM4C1294XL Hi,
I want to debug the boot_emac_flash (ethernet bootloader) project. Inside copy_loop (copying flash to SRAM), the program gets stuck. It never exits the loop.
ProcessorInit: .asmfunc
;;
;; Copy the code image…
Part Number: SW-EK-TM4C129EXL Other Parts Discussed in Thread: EK-TM4C129EXL , TM4C129ENCPDT Dear all,
I use UART2 (PA6 as Tx and PA7 as Rx). I send a data stream like 17, 03, 04, 34, 45, 65 to another board(Arduino Mega). It was successfully work. But…
Part Number: SW-EK-TM4C129EXL Hi everyone,
How can I an array element is pass through UARTCharPutNonBlocking API. My code like that
int main(void) {
int i=6; unsigned int a[6]={17,03,02,45,37,45};
MB_Port(); while(i !=0) { ROM_UARTCharPutNonBlocking(UART2_BASE…