Julian Stringer said: Disabling network interfaces doesn't seem to make any difference, and isn't consistent with the following findings.
boot_demo_emac_rom behaves slightly differently from boot_demo_emac_flash. (both from the 2.2.0.295 Tivaware…
Jeremy Li said: Sorry I do not understand
Program 1
The maximum range of pui32Data can be pui32Data[16] or pui32Data[2]
Can the range of pui32Data be 64byte in pui32Data[0-15]? The original example is pui32Data[0-1] 8byte
Hi Jeremy,
The EEPROMProgram(…
Part Number: EK-TM4C1294XL Tool/software: Hello,
Is the 32kHz crystal needed for ethernet operations?
Is the 32kHz crystal needed for correct serial 2 ethernet operations?
Thanks,
Keith
Part Number: EK-TM4C1294XL Tool/software: Hello,
TivaWare 2.1.0.12573 uses an RTOS for the net_s2e example. I am trying to locate where the equivalent Systick handler is located for this project. I have a function that I would like to call within the…
Part Number: EK-TM4C1294XL Tool/software: I would like to ask about the TI EK-TM4C1294XL evaluation board and how to use the Bootloader (Uart Update) mechanism. Currently, the problem we encounter is that we use the three bootloader examples provided…
Part Number: EK-TM4C1294XL Tool/software: Hi.
I am starting from usb_dev_cserial project to have 4 virtual serial ports.
I modify the code with 4 interfaces. Windows sees 4 virtual serial port but when
I try to use one of them nothing happens.
I can…
Part Number: EK-TM4C1294XL Tool/software: Good morning We've been using two variants of the EK-TM4C1294XL LaunchPad beds for a few years now in development. The first uses the Ethernet connection to read commands from the host then stream data from…
Part Number: EK-TM4C1294XL Tool/software: Hi
CAN communication using EK-TM4C1294XL as the slave receiving mode. I downloaded the sample code (spna245.zip) according to spna245.pdf, executed [simple_can_rx] on the receiving side, and confirmed that communication…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: EK-TM4C123GXL , MSP430FR2353 Hi,
We confirmed CAN communication using EK-TM4C1294XL as the master and EK-TM4C1294XL as the receiving node. I downloaded the sample code (spna245.zip) according…
Part Number: SW-EK-TM4C1294XL Other Parts Discussed in Thread: UNIFLASH I have LMflash programmer and Uniflash s/w installed on my windows laptop. I see erase option but is there a way I can download the image on the MCU?