Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505 Hi Team,
Posting on behalf of our customer.
I'll share this E2E post with our customer so he can reply when needed.
I am currently working on I2S communication between an EFR32 device…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505 Setup Detail
We are using the TAS2505EVM for our proof-of-concept. When the EVM runs in standalone mode , everything works correctly.
However, when we connect an external I²S master…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505 , , TAS2020 Hello Texas Instruments Support Team,
I am currently working with the TAS2505 amplifier and have noticed a clear popping/clicking noise when powering down the amplifier after…
Part Number: TAS2505EVM Tool/software: When SPKVDD=5V and an 8Ω 2W speaker is at maximum volume, what is the average DC current supplied to SPKVDD (Ispkvdd)?
This EVM board can be used with a USB 2.0 port, so I'm assuming Ispkvdd is less than 500mA…
Part Number: TAS2505EVM Hi Ti team,
After connecting the TAS2505EVM board to the computer, I opened the Codec Control software, which displayed the connected device, and then clicked View ->Example Configuration... -> The progress bar on the Playback…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505 Tool/software: The speaker output waveform was output using the evaluation board. The resulting speaker output waveform was a square wave.
Regardless of the volume, the amplitude voltage…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505 Tool/software: TAS2505EVM
TAS2505
=====my specification ======
SPK: use
HPOUT : not use
SPKVDD:5V
AVDD and DVDD: internal LDO 1.8V
IOVDD:3.3V
Speaker Impedance: 8ohm
=…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505
Tool/software:
Hello, when I was using TAS2505, I noticed the 1.8V output port from the LDO produces about 2.7V if I connect the board via USB or provide a 5V voltage externally, and…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505-Q1 , TAS2505
Tool/software:
==≈======================
My specifications and register settings
OutDAC: Class D
Input : TDM or I2S
Speaker load: 8Ω/2W
SPKVDD: 5V MCLK frequency…