Part Number: TCA39306
Are there any problems if the power supply is as follows ?
- VREF1 :+1.2V
- SCL1/SDA1 Pull-Up Voltage : +3.3V
I2C Controller IO voltage is variable (1.2V – 3.3V).
Part Number: TCA39306 TCA39305 support team
Figure 9-2 is recommended for controlling SW enable.
Is it possible to directly connect VREF2 and EN terminal to GND for SW control as shown below?
If NO, why is it?
Thanks
Tamio
Part Number: TCA39306 Other Parts Discussed in Thread: TCA9617A Hi Team,
Does TCA39306 have repeater function? It is not clear in datasheet.
If yes, what's the advantage comparing with TCA9617A?
Thanks.
Part Number: TCA39306 Other Parts Discussed in Thread: SN74AXC1T45 , LSF0101 Hi, TCA39306 support team
I would like to use the TCA39306 for GPIO, not for I2C. Now, I'm thinking of using only the SCL1/SCL2 pins and leaving the SDA1/SDA2 pins unused. …
Part Number: TCA39306-Q1 Other Parts Discussed in Thread: TCA39306 , TXS0102-Q1 , TXS0102 Hello Team,
I only found there is a description about TCA39306 can support 12.5MHz on i3c. Can I confirm if it can support such high frequency on MDIO?
If not, do we…
Part Number: TCA39306-Q1 Hi All,
I could not find the AEC-Q100 word in the D/S of the TCA39306DCURQ1 . May I know whether this device passes the AEC-Q100 testing? Need your confirmation on this part. Looking forward to your reply. Thank you.
Part Number: TCA39306-Q1 Other Parts Discussed in Thread: TCA39306 , TCA9800 , , TCA9801 I am designing a circuit that interfaces with an FPGA (1.5V LVCMOS IO) and a clock generator (3.3V I/O) through I2C. I am familiar with the Analog LTC4301 and LTC4313…
Part Number: TCA39306 Hello TI
I have to do the translation for where one side varies from 5V (USB Charger)to 3.7V(Battery) at Vref2 and another side is fixed at 3.3V(Vref1,LDO Output). I want to Control the EN pin using 3.3V (Voltage at Vref1) instead…
Part Number: TCA39306 Other Parts Discussed in Thread: PCA9306
Hi INT team,
I am designing with the PCA9306 or TCA39306 and I was curious about the switch/EN capabilities of the device.
In the datasheet it calls out the Switch Mode vs the Translation…