Part Number: TCA6408A-Q1 Other Parts Discussed in Thread: TCA6408A Is the TCA6408A-Q1 capable of producing a low frequency PWM signal with good accuracy on the duty cycle? The frequency would be less than 400Hz and the duty cycle accuracy is assumed to…
Part Number: TCA6408A-Q1 Does the TCA6408A-Q1 I/O expander support 5V slave voltage? The product overview list of I2C IO expanders on the TI site says this component is rated for 5V slave voltage, but the datasheet says 3.6V. Anyone know which one it…
Part Number: TCA9555 Other Parts Discussed in Thread: TCA6408A-Q1 , TCAL6408 , TCAL9538 , TCAL6416 , TCAL9539 Tool/software: Hi expert,
Could you help recommend a replacement for TCA9555PWR for a wider operating temperature (over 85℃)?
Joyce
Part Number: TCA6408A-Q1 Champs,
So if I power the VDDP pin with 1.8V on the TCA6408- can I have pullups to 2.8V if configured in open-drain mode? Normally I would have said this is a no-no in IC design; but if its truly open drain then maybe this works…
Part Number: ULC1001 Other Parts Discussed in Thread: TCA6408A-Q1 Tool/software: If my host I2C is 1.8V and I want to link I2C with ULC1001 that just only use 3.3V. Should I add level shift IC to contact I2C wiht ULC1001 ?
And add use TCA6408A-Q1 that…
FAQ: Logic and Voltage Translation > IxC >> What I2C IO Expanders Support Automotive Grade 1?
There are a total of 3 to date.
TCAL9539-Q1 - 16-bit, 1.08V to 3.6V I2C IO Expander, single supply, interrupt, reset, Agile I/O Configuration
TCA6408A…
Hi Xiwen,
IO levels follow VCC according to your explanation.
If you need separate logic levels for the I2C and GPIO level side, then consider the TCA6416A or TCAL6416.
Given you are looking at an automotive part, we do not have TCAL6416 or TCA6416A…
Part Number: TCA9539-Q1 Other Parts Discussed in Thread: TCA9535 , TS5A23157-Q1 , TCA9548A-Q1 , TCA6408A-Q1 , TCAL9539-Q1 ,
Hi,
please suggest part with the same specifications & standards with having of 3 address bits
thanks in advance
Part Number: TCA6408A Hi all!
I was using the tca6408A UQFN package in my design.
As it stands, there are no TCA6408A available in any package...
I noticed the tca6408A-Q1 (TSSOP package) - Can anyone tell me if it is a direct alternative? if not…