Part Number: TCA9517A Other Parts Discussed in Thread: TCA9517 Tool/software: Hi Tyler about thr TCA9517A Bside Has this been repeated across multiple TCA9517A's?
Yes, it does I just want to make sure in the simulation and the measurement different…
Part Number: TCA9517A Other Parts Discussed in Thread: TCA9517-Q1 , TCA9517 Dear Technical Support Team,
I belive that TCA9517A can supply for “VCCA > VCCB”. However TCA9517A website states “Supply restrictions: VCCA ≤ VCCB”.
Is this typo?
According…
Part Number: TCA9517A Other Parts Discussed in Thread: TCA9517 Tool/software: Hello,
I have a 5V micro-controller and only one I2C bus, and a remote 3.3V sensor, between them about 0.85m long wires, so I'd like to add I2C buffer to isolate sensor from…
Part Number: TCA9517A Other Parts Discussed in Thread: TCA9517 Tool/software: ◆Q uestion
This device (TCA9517A) and the TCA9517 have the same terminals.
Are the internal specifications the same?
Is the TCA9517A a suitable replacement for the…
Part Number: TCA9517A Other Parts Discussed in Thread: TCA9803 , TCA9509 Hi,
I am looking for an I2C buffer alternative for TCA9517A, which has
internal pull-ups on one side which get disconnected or high impedance when the VCC is off
no internal…
Part Number: TCA9517A Other Parts Discussed in Thread: LSF0002 , TCA9800 , ISO1640 , TCA4311 , TCA4307 , TCA9803 , TCA9511A , TCA9617B Hi Sirs,
Take a TI.TCA9517A to be reference, and write my design requirement as lists :
(1) Operating supply voltage…
Part Number: TCA9517A Hi, I am evaluating using TCA9517A as I2C buffer, between two modules powered by 3.3V, but one side (A) is constantly powered while the otherside (B) can be powered off.
TCA9517A 's datasheet says
High-impedance I2C pins when…
Part Number: TCA9517A Tool/software: Hi Expert,
This is Shenzhen FAE Evan. My customer use TCA9517A as a buffer between system SOC I2C port and external HDMI I2C port as shown in the schematic below. And A side is connected to external HDMI port, B…