Part Number: TCA9534 Hello,
We are planning to use the TCA9534PWR 8-bit I/O expander in our design.
We would like to confirm the expected product lifecycle and long-term availability of this part. Please let us know if there are any planned EOL/NRND…
Part Number: TCA9534 Tool/software: Hi,
I use the Arduino_UNO to control the chip TCA9534PWR and it can work but it have a have a big glitch on data pin.
the glitch is a 1.7MHz puls and my cloxk is 50KHz, Add The RC filter is not work.
Could you…
Part Number: TCA9534 Other Parts Discussed in Thread: TCA6408A Tool/software: I found out TCA6408A has an additional current in standby mode of around 25uA. I could not find a parameter like this for TCA9534 . Does that mean it doesnt exist? I need it…
Part Number: TCA9534 hi,
I would like to know if I set the not connected I/O pins to output low , the power consumption will be under 1uA ? and if I set them to output high ? or to have the minimum power consumption I have to set them in input with…
Part Number: TCA9534 Other Parts Discussed in Thread: TCAL9539 , TCA9535 , TCA9543A , TMUX136 Tool/software: Hello guys,
One of my customers is considering using TCA9534 for their new products.
At this moment, they have the following question.
Could…
Part Number: TCA9534 Sir,
I request a detailed register map specification for the the GPIO Expander TCA9534. We are attempting to control the GPIOs from a Raspberry PI.
Thanks,
Rajesh
Part Number: TCA9534 Hello Expert,
We are using TCA9534PWR, TCA9535PWR now.
When we checked block diagram, we can't find TVS Diode internally.
Do these devices have some TVS Diode internally?
I f not, do you have any recommended part which is…
Part Number: TCA9534 Hello,
I am using tca9534 as my IO expansion port to control a digital tube, now I have configured all the IO ports as output ports, I can set these IO ports to the number I want, I have read the datasheet of tca9534, I only need…
Part Number: TCA9534 Hi team,
I would like to ask about the Low-level input max voltage of TCA9534PWR. I see in the datasheet there are 2 Low-level input max voltage corresponding to 2 Vcc range:
So when I supply Vcc = 3.3V, what is the Low-level…