Part Number: TCA9535
We are using the TCA9535RTWR IC in our product. I have attached the image for your reference.
As shown in the figure, ports P15, P16, and P17 are tied to GND with 100k pull-down resistors.
Can we remove the pull-down resistors…
Part Number: TCA9535 Tool/software: Hi Team,
The datasheet requires ticf & tocf as below. based on VCC = 3.3V, the min ticf and tocf is ~12ns.
While the real test in my customer board is 3ns. is there any risk? if yes, how to remove this risk? …
Part Number: TCA9535 Other Parts Discussed in Thread: PCF8574 , TCA9554 , TCA9554A , TCA9555 , PCF8574A , PCA9554A , PCA9555 , PCA9554 , PCF8575 Tool/software: hi team
could u kindly help to review the schematic? thanks!
Part Number: TCA9535 Other Parts Discussed in Thread: TCA9555 , Tool/software: Hi Team,
Question from Nvidia, TCA9555 is pulled up by internal resistor during POR. Can you confirm the internal pull up resistor during POR (inside IC)? Thanks!
Part Number: TCA9535 Other Parts Discussed in Thread: TCA9539-Q1 Tool/software: Hi Team
I'm pretty sure the answer is yes but was hoping to get confirmation. Can I pull-up the INT output to +3V3 while the remainder of the IC operates from +5V?
Also…
Part Number: TCA9535 Tool/software: Hi Team,
I am looking for a I²C Portexpander with the following requirements:
3.3V Supply
In total we need 16 Outputs and 4 Inputs (at the moment I would use two TCA9535)
High output current would be beneficial…
Part Number: TCA9535 Other Parts Discussed in Thread: TCA9539 , , TCAL9539 , TCAL6416 Tool/software: Some GPOI devices have newer superior successors, for example the TCA9539 now has a 1MHz lower voltage TCA L 9539 counterpart, which also has more nice…
Part Number: TCA9535 Tool/software: Hi,
Problem Description: We are using TI Expander (TCA9535) in our production line, with a VCC of 1.8V. Due to a new project design with weaker Pull down driving, we found that after voltage division with the expander…
Part Number: TCA9535 Other Parts Discussed in Thread: IO-EXPANDER-EVM Hello TI Team,
I am referring to the I/O Expander User Guide , specifically Chapter 5.3 (Flashing procedure), points 8 and 9 , which describe the steps for flashing.
During this…
Part Number: TCA9535 HI.experts
The project is planned to be designed using the TCA9535 and is expected to use 8 TCA9535s.I read the technical manual (SLVA689).There are some questions in the documentation, please help with them.
1、How is the value…