Part Number: TCA9539 Tool/software: Dear TI Team:
I just want to check IO expander_TCA9539RTWR output status.
When one Port of TCA9539RTWR is set to output, it will have 3 status: High,low, and High impedance , Right?
Best Regards
Lisa
Part Number: TCA9539-Q1 Tool/software: HI TI,
How should we deal with unused pin of TCA9539-Q1? What is the reset state of these pin? Can we just left it float?
BR
Junsong Gu
Part Number: TCA9539-Q1 Tool/software: Hi Expert,
May I ask
1. How TCA9539QPWRQ1 handles interrupt signals when receive them, regardless of whether they are level triggered or pulse triggered?
2. How TCA9539QPWRQ1 handles when it is edge triggered? Will…
Part Number: TCA9539-Q1 Other Parts Discussed in Thread: TCA9539 Tool/software: Dear team,
If all ports of TCA9539 are set to output mode, then the INT pin has no meaning. Can the INT pin be left unconnected? Thanks!
Regards,
Mingkang
Part Number: TCA9539-Q1 Other Parts Discussed in Thread: TCA9539 Tool/software: Hi team,
Do we have Linux driver for TCA9539-Q1 can share with customer? Or do we have reference code which can help customer implement in Linux driver?
Thanks!
Ethan We…
Part Number: TCA9539-Q1 Tool/software: How much current of TCA9539-Q1 VCC? How to understand 160mA? In 6.5 and 6.9 chapter, ICC is not over 1mA, is in uA level, my question is, when calculate power current, which current is right?
Part Number: TCA9539 Tool/software: Dear TI Support Team,
I am contacting you regarding an ESD susceptibility issue observed with the TCA9539PWR IO Expander. During internal testing, the device fails to pass our ESD Air Discharge test at ±10KV, with…
Part Number: TCA9539 Tool/software: My SDA and SCL line have a 3.3 volts level and my TCA9539 is powered by 1.8 volts. It works but I dont know if there is a risk od damage. The datasheet is not clear if it is aceptable or not. Can you help me? Than…