Part Number: TCAN1044AV-Q1 Tool/software: Hello Ti Team,
Wanted to understand the STB mode in detail.
Is it possible to configure / switch between Normal and Standby Mode by using external switch circuit such as Transistor or MOSFET instead of uC.
Part Number: TCAN1044AV-Q1 Tool/software: How do we select the value of CMC to be used in the differential lines ? Which is best 100 or 51uH? What is the calculation to be done , to get the value of inductor ?
Part Number: TCAN1044AV-Q1 Tool/software: Hi Team,
I am using TCAN1044AVDRQ1 CAN transceiver in one of my design. The below is the screenshot of circuit. I have connected 1.8V supply voltage for VIO pin. Is 1.8V voltage is acceptable on VIO pin?
I am…
Part Number: TCAN1044AV-Q1 Tool/software: Hi team,
What are the differences between TCAN1044VDRBRQ1 and TCAN1044AVDRBRQ1? Are the dies the same? What changes have been made to the chip?
Please help answer.
Part Number: TCAN1044AV-Q1 Tool/software: Hello experts:
I have a question about the interface products' common voltage . The RS-485 common voltage usually from -7 to 12V , and the CAN interface usually from +-12V. My question is why need to support…
Part Number: TCAN1044AV-Q1 Tool/software: Hello, If the CANH or CANL signal becomes a ground fault/sky fault during communication, could the VCC (5V) pin have excessive current flow and the TCAN1044AV-Q1 device could be damaged? Or some kind of protection…
Part Number: TCAN1044AV-Q1 Tool/software: Hello, My customer has a question. At TCAN1044AV-Q1, how much time does it take from Falling undervoltage detection to getting into a protected state? Best regards, K.Hirano
Part Number: TCAN1044AV-Q1 Hi Team,
My customers are using TCAN1044AV-Q1 in their projects and facing some issue when doing the EMI/EMC tests. As you can see during the radiation test the results on 30MHz and around 90MHz is a little bit higher.
For the…