Part Number: TCAN1044AV-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 ・Does the TCAN1044AV operate without connecting VIO?
(I think the TCAN1044AV does not work properly because the RXD logic circuit does not work.)
・Can the VIO of the TCAN1044AV…
Part Number: TCAN1044AV-Q1
Hi Sir,
My customer meet a problem with the standby mode, why the RXD is providing the incorrect waveform after engine-ON?
Why are there not see any wake-up waveform? cause the system can not going to the normal mode.…
Part Number: TCAN1044AV-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 , AWR1843 Hi Team,
It looks like TCAN1044A-Q1 can not support 3.3V system.
If I want to connect MCU which is 3.3V system in AWR1843 , the TCAN1044A”V”-Q1 is the only solution…
Part Number: TCAN1044AV-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 Hi team,
Could we leave VIO floating pin or have to connect to I/O logic supply?
I know TCAN1044A-Q1 has NC pin and TCAN1044AV-Q1 has VIO. For flexible design, we would like…
Part Number: TCAN1044AV-Q1 HI,
We have one design with TCAN1044AVDRQ1 CAN transceiver. During standby operation , Device is unable to wake once we give WUP pattern. While on same hardware when we tested TCAN1042AVDRQ1 ,host controller is wake up.
…
Hi Alan,
1. Do you mean the abs max rating of CANH/CANL pin? Those are thresholds cannot be exceeded. There is no time limit as long as the voltage is within the abs max rating.
2. TCAN1044AV-Q1 uses a newer technology hence the price is lower, it…
Part Number: TCAN1044A-Q1 Tool/software: Hello,
we use the TCAN1044AV...Q1 in applications with 3.3V power supply on the µC. (Vio pin (5) = 3.3V; VCC pin (3) = 5.0V). Is it possible to use the same device ( TCAN1044AV...Q1) in applications with only…
Hi Tendulkar,
You may also see TCAN1044AV-Q1 or our newer lower supply devices like TCAN3404-Q1 (See Overview of 3.3V CAN Transceivers ), thanks.
Best Regards,
Michael.