Part Number: TCAN1046-Q1 Tool/software: Hi Expert,
Have a nice day.
For TI’s CAN device, what is the max channel? Just 2 channels?
Best Regards,
Leo Ma
Part Number: TCAN1046-Q1 Other Parts Discussed in Thread: TCAN1046A-Q1 Tool/software: Hello team,
Do you recommended solutions or device to achieve multi CAN device access, in gateway application, there are up to 10x CAN in system, how to access certain…
Hi Eric,
We have a concern with "TCAN1046-Q1". Referring to datasheet of "TCAN1046-Q1", it seems it has only one power pin i.e VCC and as per electrical characteristics, supply between 4.5V and 5.5V is expected. Even the VIH,VOH parameter on TXD and…
Part Number: TCAN1046-Q1 Other Parts Discussed in Thread: TCAN1046V-Q1 , Hi Team,
Customers want to know howTCAN1046 must do to make TX and RX levels at 3.3V?
Please help to answer how to set, THX
Part Number: TCAN1046-Q1 Hello TI Team
We are planning to use TCAN1046-Q1 dual transceiver part with dual can controller of NXP.
Our requirement CAN transceiver should support both SAE J1939 and ISO 11898 standards, as we not got that information…
Part Number: TCAN1046-Q1 Other Parts Discussed in Thread: MANDO I'm SJ Park in part dev. team / HL Klemove(Previously Mando hella electronics)
We are using TCAN1046DMTRQ1 part for our application.
When we checked AEC-Q100 report, There is no PTC test…
Part Number: TLIN1024A-Q1 Other Parts Discussed in Thread: TCAN1046-Q1 , , TCAN1046A-Q1 Hi team,
Our customer is looking into the TLIN1024/TCAN1046 datasheet and it seems there are some difference in recommended schematics/layout.
For example in TLIN1024…
Other Parts Discussed in Thread: TCAN1046-Q1 Dear Team,
Customer is looking for one channel input and two channel output CAN.
For 3.3V, 250k, SMD type and non-isolated.
Do we have suitable solution here?
BR
Kevin