Part Number: TCAN1051H-Q1 Other Parts Discussed in Thread: ISO1042 Hello,
We are using the TCAN1051HDQ1 in an isolated CAN circuit. The isolation is performed with a pair of opto-couplers which isolate the RxD and TxD signals. The RxD signal of the…
Part Number: TCAN1051H Dear Team,
Customer would like to replace TJA1051 with TXD to RXD within 200ns
Is the spec. I provide below correct to compare NXP's spec.?
Be
BR
Kevin
Part Number: TCAN1051H Other Parts Discussed in Thread: TCAN1051 Hi Sir
May we know if TCAN1051HD can direct replace MAX13053A?
I saw TCAN1051HD have FD function, is it a benefit?
Bogey
Part Number: TCAN1051H Other Parts Discussed in Thread: STRIKE Hi, Could you tell me about ESD Ratings? Is there an ESD Rating spec between CANH and CANL? Should I check “All terminals”? Best regards, Yuto Sakai
Part Number: TCAN1051H Other Parts Discussed in Thread: TCAN4550-Q1 Hi team,
My customer wants to find the solution to replace the mcp2518 which is a SPI to CAN device. Do you have some suggestions to recommend? Thanks.
Part Number: TCAN1051H Hi,
my customer is using this device for board to board communication. The distance is just around 10cm.
There are only 2 TCAN1051H in the system.
Part Number: TCAN1051H-Q1 Other Parts Discussed in Thread: TCAN1051-Q1 , TCAN1042-Q1 Hi Team,
Could you let me know when will we use the silent mode(TCAN1051-Q1) and standby mode(TCAN1042-Q1)?
Regards,
Roy
Part Number: TCAN1051G-Q1 Other Parts Discussed in Thread: TCAN1051-Q1 , TCAN1051H-Q1 Hi:
Vbus=40V
Vcc=0V
Any different leakage between TCAN1051-Q1 and TCAN1051H-Q1? Or same leakage current?
Part Number: TCAN1051H Dear Sir
I can't download TI design tidub36a on TI website ,could you kindly help to provide this data
I would like to know how to design ESD for CAN Bus
Thanks
Part Number: TCAN1051H Hi Team,
Good morning, do we have a TVS diode recommendation for CAN buses with higher battery voltages, around ~60V (instead of the traditional 12V/24V) for use with the TCAN1051H?
Looking at the IEC61000 transient protection…