Part Number: TCAN1051HGV Hi
We are using the TCAN1051HGV in product and want to add an external TVS on the CAN-L/H data lines as suggested as an optional additional protection in the datasheet.
The datasheet lists the following absolute maximum ratings…
Part Number: TCAN1051HGV Other Parts Discussed in Thread: TCAN1051HV Hi Team,
I had a few questions regarding the TCAN1051HV or TCAN1051HGV.
What is the slew rate of the output?
Are any special measures needed in order to meet emissions and immunity…
Part Number: TCAN1051HGV Hello,
My customer would like to use TCAN10xx Controller Area Network (CAN) Evaluation Module: http://www.ti.com/tool/tcan1042devm#buy to test TCAN1051HGVDR.
Is it something feasible? Because in the product folder I see this…
Part Number: TCAN1051HGV-Q1 Other Parts Discussed in Thread: TCAN1051HGV Hi,
I need to interface this CAN bus transceiver with an FPGA that uses a standard LVTTL 3.3V logic. I read that components with the "V" suffix have a voltage shifter.
Can…
Part Number: TCAN1051HGV-Q1 Other Parts Discussed in Thread: TCAN1051 Hi ,
I amd wondering if our device TCAN1051 support also the shield mode. It is not really describe in the datasheet :
" The proposed CAN FD Shield transceiver provides three operation…
Hi Kazuya,
The eight industrial TCAN devices are the TCAN1051H, TCAN1051HG, TCAN1051HGV, TCAN1051HV, TCAN1042H, TCAN1042HG, TCAN1042HGV, TCAN1042HV. Here is the URL for each part:
TCAN1051: www.ti.com/.../tcan1051hv
TCAN1042: www.ti.com/.../tcan104…