Part Number: TCAN1051HV-Q1 Other Parts Discussed in Thread: ISO1042-Q1 , , TCAN1051HV , STRIKE
Hi TI Team,
We have two PCB variants of the same design in which we use the TCAN1051HV-Q1 (Non Isolated) & ISO1042-Q1 (Isolated) parts (schematic as shown below…
Part Number: TCAN1051HV-Q1 Other Parts Discussed in Thread: TCAN1051HV , TCAN1051 Hi,
please conform following features are available in the TCAN1051HV?
CAN interface allows for compliance with both CAN Open and CAN J1939.
CAN bus shall be a CAN 2.0b…
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: TPA3116D2-Q1
Hi,
We are using TLV320AIC3104-Q1, TPA3118D2QDAPRQ1 and TLV320AIC3100IRHBR in Audio section,
Please find attachment schematic.
Please review all three Pages of schematic, please…
Part Number: TCAN1042HV Hi,
Please find attachment PDF for CAN schematic, please review and let us know if any changes need to be done
Thanks
Sagar
CAN.pdf
Part Number: TCAN1051HV-Q1 Hi Sir/Madam,
We are currently using TCAN1051HVDRQ1 in our design. We would like to test the Bus Fault protection up to 60V of the part. What is the timing of the 60V voltage level we can provide to IC without damaging the…
Part Number: TCAN1042HV-Q1 Other Parts Discussed in Thread: TCAN1051HV-Q1 , , TCAN1051 At present i am using TCAN1051HV-Q1 in my design as CAN interface. We have a plan to develop alternate for ease of procurement.
i checked all the parameters with TCAN1042HV…
Part Number: TCAN1051HV-Q1 Other Parts Discussed in Thread: TCAN1051
We have seen Both CAN FUSE open and ESD diode failure in field . In all cases this failure happened only during Charger Grid. attached block dia FYR Supply disconnection or making&Breaking…
Part Number: TCAN1051HV-Q1 HI Team,
Do we specify the max voltage for the CANH/L to device ground?
What's the voltage for the internal TVS of the CANH/L if there is?
And also how to select the external CANH/L TVS?
Do we have any guidance?
Thanks …
Part Number: TCAN1051HV-Q1 Other Parts Discussed in Thread: TCAN1051 , TCAN1051HV , STRIKE , LM5060 , LM5008 , LM5116 1. Do you have a comparison data for transmission performance or EMC of TCAN1051 with and without common mode choke?
2. For TCAN1051HV : Ex…