Part Number: TCAN1057A-Q1 Hi Team,
Customer would like to know the ESD capability of VCC pin . They met a EOS issue when using competitor.
Thanks in advance.
BRs,
Francis
Part Number: TCAN1057A-Q1 Should the absolute maximum rating for the TxD pin be interpreted from the datasheet's V(Logic_input) specification? Also, is it acceptable for a voltage to be applied to the TxD pin before VCC is supplied, to avoid false dominant…
Part Number: TCAN1057A-Q1 Tool/software: Hello,
We are using TCAN1057A-Q1 as the 5V UART-CAN converter interfacing with TI TPS929240 LED driver,
for EMC purpose we may require to put 1nF to 2.2nF MLCC capacitor on TCAN1057A-Q1 RX/TX pin.
Since…
Part Number: TCAN1057A-Q1 Dear TEXAS INSTRUMENTS Team, I hope this message finds you well. I Want TCAN1057AVDDFRQ1 this Product IBIS Model. Could you please Share Them. Thank you for your time and support. I look forward to your response. Best regards…
Part Number: TCAN1057A-Q1 Product : TCAN1057AVDRQ1
I need the following information to register new electronic parts in my company.
1) Lead and electrode plating specifications (including thickness)
note: The composition ratio of plating should…
Part Number: TCAN1057A-Q1 Hi,
When I used the TCAN1057A-Q1 chip to develop PCAN, the chip could only run up to 4M speed and could not
communicate at 5M and above. The 4M speed communication waveform edge was slow during testing,
and the chip specification…
Part Number: TCAN1057A-Q1 Hi team,
are there any concerns about having a 1uF decoupling capacitor instead of the recommended 100nF at the Vcc pin?
Best regards
Felix
Part Number: TCAN1057A-Q1 Other Parts Discussed in Thread: TCAN1057-Q1 Regarding the TCAN1057-Q1 chip in SO8 packaging, what are the foundries for its wafer fabrication and packaging/testing?
Part Number: TCAN1057A-Q1 Dear Supplier,
Good day!
We are in the process of collecting information regarding the BMW DCDC Gen Basis Project
Kindly provide the details requested below, specifically the standard used for whisker testing and confirmation…
Part Number: TCAN1057A-Q1 Dear team,
My customer is looking for CAN repeater solution. I found the reference design below and understood external logic circuit for aribtration and CAN TRX (or ISO CAN when different voltage level system connection.)…