Part Number: TCAN1146-Q1 Dear TI Experts,
I am a bit confuse about operating supply voltage of TCAN1146-Q1, as I saw the Vsup's limit votage up to 42V , but the recommmeded operating voltage only up to 28V , I don't understand why there is large votage…
Part Number: TCAN1146-Q1 Dear TI Expers,
Pls. help to check whether TCAN1146-q1 can meet all requirements of ISO11898-2:2024 ?
The datasheet only mentions it can meet all requirements of ISO11898-2:2016 …..
Whether TCAN1146-Q1 can be able to receive…
Part Number: TCAN1146-Q1 Tool/software: Hello, Referring to the questions: TCAN1146-Q1: Some bus faults are latched only for almost one second although the fault is physically applied on bus - Interface forum - Interface - TI E2E support forums
You…
Part Number: TCAN1146-Q1 Hi team:
Initialize the TCAN1146 MODE_CNTRL register to 0x01 that means enter Sleep mode and disable selective wake, but if specific data appears on the CAN bus at this time, TCAN1146 will enter standby mode(MODE_CNTRL is 0x04…
Part Number: TCAN1146-Q1 Hi, team:
At first, the CAN bus voltage was 2.3V(CANH = CANL = 2.3V), then connect another CAN device to the CAN bus, the device uses TCAN1146 as the CAN transceiver. At this time, measured CAN bus voltage is 1.6V, if the second…
Part Number: TCAN1146-Q1 Hi,team:
The following figure is from the TCAN114x datasheet:
I use a DC power supply to output 12V to VSUP while displaying the current value.
I set the MODE_CNTRL to 0x01 that is Sleep mode and selective wake is disable…
Part Number: TCAN1146-Q1 Other Parts Discussed in Thread: TCAN-SOIC14-EVM Tool/software: Hi,
I am testing the TCAN-SOIC14-EVM (Universal SOIC 14-pin CAN evaluation module) along with the AM64-SK and I would like to get a reference code to emiliano_borghi…
Part Number: TCAN1146-Q1 Other Parts Discussed in Thread: TCAN1145-Q1 Tool/software: Dear Sir or Madam,
we are currently working in the Hardware safety analysis (FMEDA) in a project that includes TCAN1146. Can you please provide me any FMEDA related…
Part Number: TCAN1146-Q1 Dear TI Expert,
We plan use TCAN1146-Q1 in our 24v system product, now we confuse wherther 1206 package terminal reistors is enough for CAN line short to battery ( voltage range is from 16 to 36V , normal voltage is 24V, loaddump…