Part Number: TCAN11623-Q1 Tool/software: Hello,
I am looking for a conformance test report according to ISO 16845 for the TCAN11623-Q1. And do you also have the conformance tests to execute on CAN? Could you please share the documentation?
Best…
Part Number: TCAN11623-Q1 Tool/software: We have populated the PCB and attempted to power up the boards. However, we are facing the following issue during the board bring-up:
After powering up, we are able to measure 3.3V for approximately 3 to 4…
Part Number: TCAN11623-Q1 Tool/software: Hello,
In order to use this device we need additional information:
Wafer size
Node size
Technology
Wafer fabrication Location
Assembly and testing location
Thank you for your support!
Silviu
Part Number: TCAN11623-Q1 Tool/software: Hello,
I'm using a TCAN11623DMTRQ1 (CAN transceiver + LDO 3.3V) with a 10uF connected on VLD03 pin GCJ31CR71C106KA15L
A 10uF with same reference is connected on VFLT
Input capacitors are 220 + 100nF…
Part Number: TCAN11623-Q1 Tool/software: Hello,
I am using a TCAN11623
According to datasheet wake up is done by the multiple filtered dominant wake up patern defined in the ISO11898-2:2016 Standard
Is this patern the same way to wake up as defined…
Part Number: TCAN11623-Q1 Tool/software: Hi team,
Our customer would like to know the dimension of Pin 1 ID of TCAN11623-Q1 below for board layout design. Could you provide the dimension for this PIN 1 ID?
Thank you,
Muwei Zheng
Part Number: TCAN11623-Q1 Tool/software: Hello Experts,
We are using TCAN11623DMTRQ1 ass our primary CAN trans receiver in our 400V & 48V BMS Project. Where it is powered by 12V and VIO-is 3.3V. During Bulk Current Injection test at LEVEL 3 (150mA at…
Part Number: TCAN11623-Q1 Tool/software: Dear Experts,
We are using TCAN11623DMTRQ1 & TCAN1044ADDFRQ1 for 500kbps CAN communication in Automotive project. Kindly let us know how to select the common mode choke between CAN_H & CAN_L. On urgent basis…
Part Number: TCAN11623-Q1 Hi Team,
I'm using TCAN11623-Q1 for CAN Bus communication in my current project. I would like to ask whether it is recommended to add a common mode choke on my CAN Bus for EMI/EMC tests. And if I don't add the choke what…