Part Number: TCAN332 Hello,
I want to know is this IC supports ISO 15765 protocol as in the datasheet only one protocol is mentioned but nothing mentioned about others. Can someone help me on this?
Part Number: TCAN332 Hi,team. I'm evaluatingTCAN332DCN in a mixed 3.3V and 5V CAN system . I use 5V CAN IC that HA13721 or R2A25416 etc. I use single termination. Probing CANH with an oscilloscope , CANH has large linging at end. I assumed that I could…
Part Number: TCAN332 Other Parts Discussed in Thread: TCAN1043 Hi all,
I have two questions about max communication distance of CAN transceiver.
1. What is the max communication distance of TCAN332 under 1MHz?
2. Is it related to supply voltage? If I use…
Part Number: TCAN332 Team, with TCAN332 Vcc at 3.3V, can 12V be applied at CANH (pin7)? The differential voltage (CANH-CANL) would be 12-0=12V.
It seems to fit the datasheet specs, but wanted to verify.
Thanks!
Viktorija
Part Number: TCAN337G Other Parts Discussed in Thread: TCAN332 , TCAN337 Would it be possible to get an IBIS model for the TCAN337GDCNR Can transceiver?
Other Parts Discussed in Thread: TCAN332 Very related to thread...We have a TCAN332 (connected to our MCU) on a bus with around 63 ohm resistance throughout bus backbone (two 120-ohm resistors on ends of bus). TCAN332 has recessive state around 1.9V, and…
Other Parts Discussed in Thread: TCAN332 Hello guys,
One of my customers is looking for a CAN transceiver which can operate with 3V~5V VCC range.
Does TI have any CAN transceiver which can operate with 3V~5V VCC range? Or does TI have any plan to release…
Part Number: TCAN332 Hi Sirs,
Sorry to bother you .
We have use TI / TCAN332DCNR IC,
Our EA test requires measurement board CANBUS signal.
1. Is there any recommended measurement method for the CANBUS signal of this IC? Please provide it ?
Or
2. It is…
Part Number: TCAN332 Application note SLLA279A provides a formula for spacing CAN nodes to get reliable transmission. The article seems to indicate that this would occur if you had a really long bus length (as in the example provided), but the resultant…
Part Number: TCAN332TCAN332 3.3V power supply, in the process of communication failure, failure mode is bus U7 pin CANL to GND impedance to varying degrees to reduce or even short circuit. Under normal power-on and non-communication conditions, the chip…