Hi Iris,
Iris Shen said: 1. Would you share the details about how to monitor the clock through GPIO1? Liang said they didn't receive your email.
I've emailed you the information as well so please pass that along to Liang.
Iris Shen said: 1. Do we…
Part Number: TCAN4550-Q1 Other Parts Discussed in Thread: TCAN4550 Tool/software: Hello team,
I have a question, in my application we use the Bus Wake via RXD_INT Request (BWRR) in Sleep Mode to detect CAN activity and wake up the host MCU using the nINT…
Part Number: TCAN4550-Q1 Hi team,
Customer has below questions of TCAN4550-Q1
When they test CAN message sending and receiving, when using the receiving FIFO, because the RX FIFO capacity is too small, when the bus load is high, the RX FIFO will be filled…
Part Number: TCAN4550-Q1 Other Parts Discussed in Thread: TCAN4550 Tool/software: Hello team,
Greeting for the day.
If use 2Mbps CAN FD, can we use 32MHz crystal?
On the other hand, what need to consider when select crystal, Is the higher the Crystal frequency…
Part Number: TCAN4550-Q1 Other Parts Discussed in Thread: TCAN4550 Tool/software: Hi team,
My customer has two questions about TCAN4550:
1. Does TCAN4550's communication support trigger interrupt? If it does, what configuration is needed to do for TCAN4550…
Hi Anand,
Anand Kulkarni said: I have attempted to read and write to the registers using the functions provided in the driver code. However, despite successfully writing to the Test register, the value read from the register remains at 0.
Are you referring…
Part Number: TCAN4550-Q1 Other Parts Discussed in Thread: TCAN4550 Tool/software: Hello,
I completed the TCAN4550 initialization refer to the TCAN demo, but when I called the function
TCAN4x5x_MCAN_ClearInterruptsAll // Resets all MCAN interrupts (does…
Part Number: TCAN4550-Q1 Other Parts Discussed in Thread: TCAN4550 Hi TI Team,
In our device, we are using 2# TCAN4550RGYRQ1 IC for CAN communication,
Normally we do not face any issues with communication.
After waking up we are not receiving CAN data…
Part Number: TCAN4550-Q1 Other Parts Discussed in Thread: TCAN4550 Tool/software: Currently, the power supply is powered on board, and then VIO is controlled by MOS tube to power on after Vsup, but it seems to be powered on later than Vccout, I am not…
Part Number: TCAN4550-Q1 Tool/software: I used tcan4550-q1 and set 32 tx buffers in queue mode according to the official demo.
After writing 32 frames message with the same id to the corresponding MRAM, write 0xFFFFFFFF to the txbar(0x10D0) to request…