All right, I'll open a new thread. Thanks for the links provided, I'll have a look at them. Since I'm going to start with my application now, I prefer the opinion of experts who can provide me with products that are not obsolete in time and who…
Part Number: TCIEVMK2X Hi, all
I have two EVMK2H boards(Rev 4.0) suddenly can not start up. Both of these board have BMC error message "The signal SOC_POWER_GOOD has failed to assert".
Board 1 BMC output below message:
Boa…
Part Number: TCIEVMK2X Hi,
we are observing ASCII extended character 193 instead of 67 for CCCC in Uart mode in a K2K board.
We observed the clock to be ok. we are able to see the Sys_clock input to processor is ok. the CDCM6208 is also giving PLL Lock…
Part Number: TCIEVMK2X Issue : build is not happening with example design. it is showing following error.
Issue : In debug perspective mode, after loading the example design, example design is giving following error.
Kindly provide some solution.
Part Number: TCIEVMK2X We need help on Ti6638 SoC platform. We are working on LTE Phy layer based on Ti6638 SoC platform.
This LTE phy layer is based on lteLib library which is provided by TI. We have binary setup file (ltelib_3.0.9.0_rel10.run) for this…
Part Number: TCIEVMK2X Hi,
Recently, I want to visit the website of MCSDK wiki. But it warn me this page have been removed
http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Downloads
Does anyone know what is the new website address for this…
A support member sent me this link: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/547215/evmk2h-schematic?tisearch=e2e-sitesearch&keymatch=TCIEVMK2X%2520schematic#
Part Number: TCIEVMK2X HI,
I want to configure the AIF2 Timer event as the trigger for EDMA3 transfer. The reference has been the example projects of EDMA3 and AIF2.
The request channel fails when I give chId as EDMA3_DRV_HW_CHANNEL_EVENT_22.
EDMA3_DRV_requestChannel…
Part Number: TCIEVMK2X
I am trying to build a project using the EDMA3 LLDs. The code is as below, and the compilation errors are also attached. The same structures in the echo function, if defined globally, do not return errors. Why does this happen? …